Zoom-In feature with i.MX53 IPU - WEC7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Zoom-In feature with i.MX53 IPU - WEC7

跳至解决方案
1,858 次查看
Ashfaque
Contributor II

Hi all,

We need to extend the CAMAPP DirectDraw application to provide Zoom-In and Zoom-Out feature on the video data coming from TV-IN on i.MX53 with Windows Embedded Compact 7 platform, Using IPU block.

Referring the i.MX6 data sheet, IPU has a Image Converter (IC) block which does the Image conversion related operations which also includes re-sizing and rotating.


But we are not sure on how to use this particular feature in the DirectDraw architecture level. One option would be to implement this functionality as a Direct Draw Video Port in the DirectDraw HAL layer. currently HAL layer does not have any implementation related to these features.

Please let me know any ideas regarding to this.

Regards,

Ashfaque

标签 (3)
标记 (2)
0 项奖励
回复
1 解答
1,634 次查看
yossishukron
Contributor III

you can use the PP there is a user level interface to access the PP.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,635 次查看
yossishukron
Contributor III

you can use the PP there is a user level interface to access the PP.

0 项奖励
回复