Zigbee interfacing with i.mx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Zigbee interfacing with i.mx6

1,912 Views
jithcrcr
Contributor I

Hi,

Does i.MX6 processors interface with Zigbee module JN5168-001-M05?

Have you tested Zigbee in SabreSD on Android?

Labels (4)
Tags (2)
0 Kudos
Reply
1 Reply

1,437 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

I’m afraid that there aren’t any reference material specifically for the Zigbee module that you are mentioning. However, you could take a look at the following links, which provides useful information about Zigbee connectivity using i.MX processors and/or Android devices:

Lighting Control Philips Hue Light Through KW20(Zigbee Coordinator) with i.MX6Q

ZigBee/Wi-Fi Connectivity Gateway for the Smart Home

Enabling Android devices to use Freescale RF4CE BlackBox for Final Application using i.MX53 tablet

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply