Zephyr instead of FreeRTOS on i.mx8 mini?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Zephyr instead of FreeRTOS on i.mx8 mini?

4,336件の閲覧回数
dav1
Contributor V

Anyone successfully running Zephyr (https://www.zephyrproject.org/) on the M4?

Team NXP,

any plans on supporting this as an alternative to FreeRTOS?

ラベル(1)
タグ(2)
0 件の賞賛
返信
5 返答(返信)

3,935件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Until now, just FreeRTOS is the available option from NXP to use with the M4 core of the i.MX8.

There are some 3rd parties that may provide additional BSPs for NXP processors. You could directly send your request to Zephyr, as they are NXP partners.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 件の賞賛
返信

3,935件の閲覧回数
dav1
Contributor V

Hi Carlos,

Any plans to support it (in the near term roadmap)?

0 件の賞賛
返信

3,935件の閲覧回数
maureen
NXP Employee
NXP Employee

Not at the moment, but the Zephyr community would welcome a contribution and help provide some guidance if you're interested to do it.

0 件の賞賛
返信

3,935件の閲覧回数
dav1
Contributor V

maureen‌ we'd really like to see this happen. 

Maybe you've seen, but there is some work done here that looks promising!

Zephyr support for NXP i.MX8M SoC · Issue #17814 · zephyrproject-rtos/zephyr · GitHub 

It would be great if someone from NXP can support reviewing it and also continue by adding additional peripheral support (not knowing how much that is supported by the NXP FreeRTOS release as of today)

0 件の賞賛
返信

3,935件の閲覧回数
maureen
NXP Employee
NXP Employee

Yes, we will support reviewing it

0 件の賞賛
返信