ZMK programming in imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ZMK programming in imx6

1,390件の閲覧回数
rohininarasipur
Contributor II

Hi, I want to program ZMK using software. But my SNV_HPLR write lock bit is set and it can be cleared only by a system reset. So how can I do this system reset? Any help is appreciated. Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,254件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rohini

system reset can be performed only with POR assertion.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信