ZMK programming in imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ZMK programming in imx6

1,371 Views
rohininarasipur
Contributor II

Hi, I want to program ZMK using software. But my SNV_HPLR write lock bit is set and it can be cleared only by a system reset. So how can I do this system reset? Any help is appreciated. Thanks.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,235 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rohini

system reset can be performed only with POR assertion.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply