Yocto4.3 occur "Logging error" when execute repo sync

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Yocto4.3 occur "Logging error" when execute repo sync

1,074 次查看
charleshuang
Senior Contributor II

Hi NXP Team,

As title, the error log are as below.

Could you provide any advise for us ?

Thank you.

 

" Fetching: 50% (8/16) 0:58 | 2 jobs | 0:26 meta-virtualization @ sources/meta-virtualization--- Logging error ---
Traceback (most recent call last):
  File "/usr/lib/python3.8/logging/__init__.py", line 1085, in emit
    msg = self.format(record)
  File "/usr/lib/python3.8/logging/__init__.py", line 929, in format
    return fmt.format(record)
  File "/home/adv/adv-release-bsp/.repo/repo/repo_logging.py", line 62, in format
    return msg if not colorer else colorer(msg)
  File "/home/adv/adv-release-bsp/.repo/repo/color.py", line 167, in f
    output = fmt % args
TypeError: not enough arguments for format string
Call stack:
  File "/home/adv/adv-release-bsp/.repo/repo/main.py", line 874, in <module>
    _Main(sys.argv[1:])
  File "/home/adv/adv-release-bsp/.repo/repo/main.py", line 850, in _Main
    result = repo._Run(name, gopts, argv) or 0
  File "/home/adv/adv-release-bsp/.repo/repo/main.py", line 294, in _Run
    result = run()
  File "/home/adv/adv-release-bsp/.repo/repo/main.py", line 275, in <lambda>
    lambda: self._RunLong(name, gopts, argv, git_trace2_event_log) or 0
  File "/home/adv/adv-release-bsp/.repo/repo/main.py", line 442, in _RunLong
    execute_command()
  File "/home/adv/adv-release-bsp/.repo/repo/main.py", line 408, in execute_command
    execute_command_helper()
  File "/home/adv/adv-release-bsp/.repo/repo/main.py", line 374, in execute_command_helper
    result = cmd.Execute(copts, cargs)
  File "/home/adv/adv-release-bsp/.repo/repo/subcmds/sync.py", line 1688, in Execute
    self._ExecuteHelper(opt, args, errors)
  File "/home/adv/adv-release-bsp/.repo/repo/subcmds/sync.py", line 1796, in _ExecuteHelper
    result = self._FetchMain(
  File "/home/adv/adv-release-bsp/.repo/repo/subcmds/sync.py", line 959, in _FetchMain
    result = self._Fetch(to_fetch, opt, err_event, ssh_proxy, errors)
  File "/home/adv/adv-release-bsp/.repo/repo/subcmds/sync.py", line 906, in _Fetch
    with multiprocessing.Pool(
  File "/usr/lib/python3.8/multiprocessing/context.py", line 119, in Pool
    return Pool(processes, initializer, initargs, maxtasksperchild,
  File "/usr/lib/python3.8/multiprocessing/pool.py", line 212, in __init__
    self._repopulate_pool()
  File "/usr/lib/python3.8/multiprocessing/pool.py", line 303, in _repopulate_pool
    return self._repopulate_pool_static(self._ctx, self.Process,
  File "/usr/lib/python3.8/multiprocessing/pool.py", line 326, in _repopulate_pool_static
    w.start()
  File "/usr/lib/python3.8/multiprocessing/process.py", line 121, in start
    self._popen = self._Popen(self)
  File "/usr/lib/python3.8/multiprocessing/context.py", line 277, in _Popen
    return Popen(process_obj)
  File "/usr/lib/python3.8/multiprocessing/popen_fork.py", line 19, in __init__
    self._launch(process_obj)
  File "/usr/lib/python3.8/multiprocessing/popen_fork.py", line 75, in _launch
    code = process_obj._bootstrap(parent_sentinel=child_r)
  File "/usr/lib/python3.8/multiprocessing/process.py", line 315, in _bootstrap
    self.run()
  File "/usr/lib/python3.8/multiprocessing/process.py", line 108, in run
    self._target(*self._args, **self._kwargs)
  File "/usr/lib/python3.8/multiprocessing/pool.py", line 125, in worker
    result = (True, func(*args, **kwds))
  File "/usr/lib/python3.8/multiprocessing/pool.py", line 48, in mapstar
    return list(map(*args))
  File "/home/adv/adv-release-bsp/.repo/repo/subcmds/sync.py", line 713, in _FetchProjectList
    return [self._FetchOne(opt, x) for x in projects]
  File "/home/adv/adv-release-bsp/.repo/repo/subcmds/sync.py", line 713, in <listcomp>
    return [self._FetchOne(opt, x) for x in projects]
  File "/home/adv/adv-release-bsp/.repo/repo/subcmds/sync.py", line 733, in _FetchOne
    sync_result = project.Sync_NetworkHalf(
  File "/home/adv/adv-release-bsp/.repo/repo/project.py", line 1361, in Sync_NetworkHalf
    and self._ApplyCloneBundle(
  File "/home/adv/adv-release-bsp/.repo/repo/project.py", line 2753, in _ApplyCloneBundle
    exist_dst = self._FetchBundle(
  File "/home/adv/adv-release-bsp/.repo/repo/project.py", line 2837, in _FetchBundle
    logger.error("%s", output)  "

标签 (1)
0 项奖励
回复
2 回复数

927 次查看
Shinici
Contributor I

I have same issue. Currently, I don't know how to fix this issue

0 项奖励
回复

1,052 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

My suggestions to follow up the section Host Setup of Yocto User Guide.

-Host package to align with the version of python.

-To delete the existed ".repo" utility and setting it up again.

-The version of Host Machine.

IMX_YOCTO_PROJECT_USERS_GUIDE.pdf 

 

Regards

Harvey

 

0 项奖励
回复