Yocto - verify rootfs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto - verify rootfs

4,034 Views
tomasklein
Contributor II

Hi,

I would like to ask, how could i verify an integrity of rootfs. I would like to create a hash or signature of rootfs and store it in for example kernel image. Uboot and zImage are already signed with HAB tool. Maybe my idea is wrong, but how could I verify integrity of my rootfs ?

PS: As build tool I am using Yocto.

Thank you, for any advice :smileyhappy:

Tags (2)
0 Kudos
Reply
1 Reply

3,678 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   NXP does not provide recommended (HAB) solutions for rootfs, nevertheless, hope, the following 

considerations may be interesting.

https://bootlin.com/pub/conferences/2018/elc/josserand-schulz-secure-boot/josserand-schulz-secure-bo... 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply