Yocto toolchain cross compile error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto toolchain cross compile error

1,791件の閲覧回数
peterchiu
Contributor II

Hi all,

Excuse me, I have an problem, I consult Freescale Yocto Project User's Guide (L3.14.52_1.1.0), and build the "meta-toolchain-qt5".

I use the toolcahin to cross compile my qt application (HelloWorld).

It's success, the Helloworld application is work in my imx6q board.

But, when  I cross compile the other qt application, it's not ok.

I got the error log:

1.jpg

2.jpg

The toolchain is use L3.14.52 to build, qt version is 5.5.

The qt application is use qt 5.4.

If anyone know what's the problem?

Please tell me. Thanks.

ラベル(3)
0 件の賞賛
返信
1 返信

1,432件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Peter Chiu,

It seems that the problem is related to link errors to libraries needed to compile rather to the toolchain itself. I would recommend looking at the libraries and .h and making sure they are referenced correctly.

Regards,

0 件の賞賛
返信