Yocto project build failed -Please confirm the installation procedure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto project build failed -Please confirm the installation procedure

9,642件の閲覧回数
bhanurajesh_bha
Contributor III

Dear Experts,

I am new to Yocto and Linux environment.

Almost spent a month of time but failed to build 

Could you please confirm the following installation procedure which i performed 

Kindly do correct me.

Thank You!

  • Step 1 : Installed Ubuntu 16.4 LTS
  • Step 2: Build Host Packages

Essentials:

$ sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib \
build-essential chrpath socat cpio python python3 python3-pip python3-pexpect \
xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev \
xterm
$ sudo zypper install dblatex xmlto

  • Step 3: Installed following packages

Git 1.8.3.1 or greater
tar 1.27 or greater
Python 3.4.0 or greater

  • Step 4

1.3.1. Downloading a Pre-Built buildtools Tarball
Locate and download the *.sh at http://downloads.yoctoproject.org/releases/yocto/yocto-2.7.1/buildtools/.

Execute the installation script. Here is an example:
$ sh ~/Downloads/x86_64-buildtools-nativesdk-standalone-2.7.1.sh
Execute the installation script. Here is an example:

$ sh ~/Downloads/x86_64-buildtools-nativesdk-standalone-2.7.1.sh

During execution, a prompt appears that allows you to choose the installation directory. For example, you could choose the following:

/home/your-username/buildtools

source /home/your_username/buildtools/environment-setup-x86-64-poky-linux

  • Step 5
    Host Packages :

Essential Yocto Project host packages are:
$ sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib \
build-essential chrpath socat libsdl1.2-dev

  • Step 6

$ mkdir ~/bin
$ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repov
$ chmod a+x ~/bin/repo
$ PATH-${PATH}:~/bin

  • Step 7

Yocto Project Setup
$ git config --global user.name "Your Name"
$ git config --global user.email "Your Email"
$ git config --list8

  • Step 7

$ mkdir imx-yocto-bsp
$ cd imx-yocto-bsp
$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m
imx-4.14.98-2.0.0_ga.xml
$ repo sync

  • Step 8

$ DISTRO=fsl-imx-xwayland MACHINE=imx8qxpmek source fsl-setup-release.sh -b build-xwayland
$ bitbake fsl-image-qt5-validation-imx

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

8,975件の閲覧回数
kunalkotecha1
Senior Contributor II

Hi bhanurajesh.bhadry@valeo.com,

You Just need to follow the steps provided in the document that is attached by you. Step 3 and Step 4 are not part of the Yocto Project User Guide. Can you please only follow the steps mentioned in the guide and let us know the error logs.

Regards,

Kunal

0 件の賞賛
返信

8,976件の閲覧回数
bhanurajesh_bha
Contributor III

HI Kunal,

I skip steps 3 & 4...getting the following error with build brek

NOTE: Your conf/bblayers.conf has been automatically updated.
Parsing recipes: 100% |######################################################################################################################################################################| Time: 0:01:13
Parsing of 2562 .bb files complete (0 cached, 2562 parsed). 3483 targets, 221 skipped, 8 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
NOTE: Multiple providers are available for runtime ptpd (ptpd, ptpd-qoriq)
Consider defining a PREFERRED_RPROVIDER entry to match ptpd
NOTE: Multiple providers are available for runtime ptpd-dev (ptpd, ptpd-qoriq)
Consider defining a PREFERRED_RPROVIDER entry to match ptpd-dev

Build Configuration:
BB_VERSION           = "1.38.0"
BUILD_SYS            = "x86_64-linux"
NATIVELSBSTRING      = "ubuntu-16.04"
TARGET_SYS           = "aarch64-poky-linux"
MACHINE              = "imx8qxpmek"
DISTRO               = "fsl-imx-xwayland"
DISTRO_VERSION       = "4.14-sumo"
TUNE_FEATURES        = "aarch64"
TARGET_FPU           = ""
meta                 
meta-poky            = "HEAD:c9bd4984f8f471ca2c43052714f4413ba99cf171"
meta-oe              
meta-multimedia      = "HEAD:8760facba1bceb299b3613b8955621ddaa3d4c3f"
meta-freescale       = "HEAD:27ca94f8a4336790ba117b4298566f6820e7e74c"
meta-freescale-3rdparty = "HEAD:82037216280a39957fb4272581637abec734ad50"
meta-freescale-distro = "HEAD:f7e2216e93aff14ac32728a13637a48df436b7f4"
meta-bsp             
meta-sdk             = "HEAD:8eeb420fad668b733ab95b460895e1c337c66b25"
meta-browser         = "HEAD:75640e14e325479c076b6272b646be7a239c18aa"
meta-gnome           
meta-networking      
meta-python          
meta-filesystems     = "HEAD:8760facba1bceb299b3613b8955621ddaa3d4c3f"
meta-qt5             = "HEAD:d4e7f73d04e8448d326b6f89908701e304e37d65"

Initialising tasks: 100% |###################################################################################################################################################################| Time: 0:00:06
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: quilt-native-0.65-r0 do_compile: oe_runmake failed
ERROR: quilt-native-0.65-r0 do_compile: Function failed: do_compile (log file is located at /home/valeo-isc/imx-yocto-bsp/build-xwayland/tmp/work/x86_64-linux/quilt-native/0.65-r0/temp/log.do_compile.11442)
ERROR: Logfile of failure stored in: /home/valeo-isc/imx-yocto-bsp/build-xwayland/tmp/work/x86_64-linux/quilt-native/0.65-r0/temp/log.do_compile.11442
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 8
| bin/quilt.in -> bin/quilt
| bin/guards.in -> bin/guards
| quilt/grep.in -> quilt/grep
| quilt/upgrade.in -> quilt/upgrade
| quilt/refresh.in -> quilt/refresh
| quilt/fold.in -> quilt/fold
| quilt/revert.in -> quilt/revert
| quilt/pop.in -> quilt/pop
| quilt/header.in -> quilt/header
| quilt/remove.in -> quilt/remove
| quilt/annotate.in -> quilt/annotate
| quilt/diff.in -> quilt/diff
| quilt/graph.in -> quilt/graph
| quilt/edit.in -> quilt/edit
| quilt/mail.in -> quilt/mail
| quilt/fork.in -> quilt/fork
| quilt/add.in -> quilt/add
| quilt/top.in -> quilt/top
| quilt/push.in -> quilt/push
| quilt/new.in -> quilt/new
| quilt/applied.in -> quilt/applied
| quilt/import.in -> quilt/import
| quilt/previous.in -> quilt/previous
| quilt/next.in -> quilt/next
| quilt/series.in -> quilt/series
| quilt/delete.in -> quilt/delete
| quilt/patches.in -> quilt/patches
| quilt/snapshot.in -> quilt/snapshot
| quilt/files.in -> quilt/files
| quilt/setup.in -> quilt/setup
| quilt/rename.in -> quilt/rename
| quilt/unapplied.in -> quilt/unapplied
| quilt/scripts/patchfns.in -> quilt/scripts/patchfns
| quilt/scripts/dependency-graph.in -> quilt/scripts/dependency-graph
| quilt/scripts/inspect-wrapper.in -> quilt/scripts/inspect-wrapper
| quilt/scripts/edmail.in -> quilt/scripts/edmail
| Segmentation fault (core dumped)
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/valeo-isc/imx-yocto-bsp/build-xwayland/tmp/work/x86_64-linux/quilt-native/0.65-r0/temp/log.do_compile.11442)
ERROR: Task (/home/valeo-isc/imx-yocto-bsp/sources/poky/meta/recipes-devtools/quilt/quilt-native_0.65.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 20 tasks of which 0 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
  /home/valeo-isc/imx-yocto-bsp/sources/poky/meta/recipes-devtools/quilt/quilt-native_0.65.bb:do_compile
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

0 件の賞賛
返信

8,976件の閲覧回数
bhanurajesh_bha
Contributor III

HI Kunal the following is the error log file

Thank You

DEBUG: Executing shell function do_compile
NOTE: make -j 8
bin/quilt.in -> bin/quilt
bin/guards.in -> bin/guards
quilt/grep.in -> quilt/grep
quilt/upgrade.in -> quilt/upgrade
quilt/refresh.in -> quilt/refresh
quilt/fold.in -> quilt/fold
quilt/revert.in -> quilt/revert
quilt/pop.in -> quilt/pop
quilt/header.in -> quilt/header
quilt/remove.in -> quilt/remove
quilt/annotate.in -> quilt/annotate
quilt/diff.in -> quilt/diff
quilt/graph.in -> quilt/graph
quilt/edit.in -> quilt/edit
quilt/mail.in -> quilt/mail
quilt/fork.in -> quilt/fork
quilt/add.in -> quilt/add
quilt/top.in -> quilt/top
quilt/push.in -> quilt/push
quilt/new.in -> quilt/new
quilt/applied.in -> quilt/applied
quilt/import.in -> quilt/import
quilt/previous.in -> quilt/previous
quilt/next.in -> quilt/next
quilt/series.in -> quilt/series
quilt/delete.in -> quilt/delete
quilt/patches.in -> quilt/patches
quilt/snapshot.in -> quilt/snapshot
quilt/files.in -> quilt/files
quilt/setup.in -> quilt/setup
quilt/rename.in -> quilt/rename
quilt/unapplied.in -> quilt/unapplied
quilt/scripts/patchfns.in -> quilt/scripts/patchfns
quilt/scripts/dependency-graph.in -> quilt/scripts/dependency-graph
quilt/scripts/inspect-wrapper.in -> quilt/scripts/inspect-wrapper
quilt/scripts/edmail.in -> quilt/scripts/edmail
Segmentation fault (core dumped)
ERROR: oe_runmake failed
WARNING: exit code 1 from a shell command.
ERROR: Function failed: do_compile (log file is located at /home/valeo-isc/imx-yocto-bsp/build-xwayland/tmp/work/x86_64-linux/quilt-native/0.65-r0/temp/log.do_compile.11442)

0 件の賞賛
返信

8,976件の閲覧回数
kunalkotecha1
Senior Contributor II

Hi bhanurajesh.bhadry@valeo.com,


We are able to build it successfully by following your mentioned steps no. 1,2,5,6,7,8.(skip the steps 3 and 4 which is not required). So, Can you please try to build by only following the steps no. 1,2,5,6,7,8.


Regards,

Kunal

0 件の賞賛
返信

8,976件の閲覧回数
bhanurajesh_bha
Contributor III

Hi,

 

Seems the problem is with Mouse Laptop.

Built on ASUS Laptop build successfully.

Thank You!

0 件の賞賛
返信