Yocto project L4.19.35 compile fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto project L4.19.35 compile fail

Jump to solution
5,254 Views
dt_liumi
Contributor I

Dear:

       Help me

        I have some problems building the system 4.19.35 for imx6q when I using the instructions i.MX_Yocto_Project_User's_Guide. I'm using ubuntu 18.04.

1、I patch according to i.MX_Yocto_Project_User's_Guide

2、The configuration information is shown in Figure 1

DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11

3、bitbake imx-image-multimedia   (this build an X11 with Qt5)

4、opencv-4.0.1.imx-r0 do_compile fail shown in Figure 2

qtbase-5.12.3+gitAUTOINC+b527725766-r0 do_compile  fail  shown in Figure 2

 

Regards

 

 

 

        

0 Kudos
Reply
1 Solution
5,230 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello dt_liumi,

It seems that you are out of memory in your host.

 

Regards

 

View solution in original post

2 Replies
5,203 Views
dt_liumi
Contributor I

Hello Bio_TICFSL

         Thank you very much

I reconfiguration VMware, Yocto project L4.19.35 Compiling, no errors occurred.

Regards

0 Kudos
Reply
5,231 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello dt_liumi,

It seems that you are out of memory in your host.

 

Regards