Yocto media device ko question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto media device ko question

1,104 Views
xu_ji1
Contributor V

Hi,

I am working on i.MX8QM yocto platform,and now I changed some media driver to ko.

CONFIG_GMSL_MAX9286=m
CONFIG_IMX8_MEDIA_DEVICE=m
CONFIG_IMX8_JPEG=m

when power on CONFIG_IMX8_MEDIA_DEVICE ko and CONFIG_IMX8_JPEG ko load by systemd,

Why camera ko not be load?which service in systemd load the media driver ko?

0 Kudos
Reply
2 Replies

998 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Xu Ji,

Is this problem still present? I would recommend looking at the default kernel configuration files as sometimes there are additional dependencies to the drivers.

If you modified the media driver then check with the manufacturer if there are additional dependencies and make sure that the required libraries are also installed.

I hope this helps.

Regards,

0 Kudos
Reply

998 Views
xu_ji1
Contributor V

hi,gusarambula

this problem still present,the media_device module and jpeg module loaded by Udev service,but camera driver module not loaded,do u know why it is like that?

0 Kudos
Reply