Yocto libc linker error while building application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto libc linker error while building application

21,094件の閲覧回数
bharathg
Contributor I

Board: imx6qsabresd

host: ubuntu 12.04

FS: yocto project 1.5 (Dora)

Description:

     When i try to compile application using poky toolchain installed via meta-toolchain, i am getting below linker errors. Please let me know how can i fix this

ERROR Log:

-------------------

/opt/poky/1.4.3/sysroots/i686-pokysdk-linux/usr/libexec/armv7a-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.7.2/ld: cannot find /lib/libc.so.6

/opt/poky/1.4.3/sysroots/i686-pokysdk-linux/usr/libexec/armv7a-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.7.2/ld: cannot find /usr/lib/libc_nonshared.a

/opt/poky/1.4.3/sysroots/i686-pokysdk-linux/usr/libexec/armv7a-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.7.2/ld: cannot find /lib/ld-linux-armhf.so.3

collect2: error: ld returned 1 exit status

Also,

While building multi-threaded gstreamer application, we are getting pthread linker errors as shown below:

ERROR Log:

-------------------

/opt/poky/1.4.3/sysroots/i686-pokysdk-linux/usr/libexec/armv7a-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.7.2/ld: cannot find /lib/libpthread.so.0

/opt/poky/1.4.3/sysroots/i686-pokysdk-linux/usr/libexec/armv7a-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.7.2/ld: cannot find /usr/lib/libpthread_nonshared.a

collect2: error: ld returned 1 exit status

ラベル(3)
タグ(4)
7 返答(返信)

7,663件の閲覧回数
bharathg
Contributor I

Below is my code test.c:

-----------------------------------

#include <pthread.h>

#include <stdio.h>

/* this function is run by the second thread */

void *inc_x(void *x_void_ptr)

{

/* increment x to 100 */

int *x_ptr = (int *)x_void_ptr;

while(++(*x_ptr) < 100);

printf("x increment finished\n");

/* the function must return something - NULL will do */

return NULL;

}

int main()

{

int x = 0, y = 0;

/* show the initial values of x and y */

printf("x: %d, y: %d\n", x, y);

/* this variable is our reference to the second thread */

pthread_t inc_x_thread;

/* create a second thread which executes inc_x(&x) */

if(pthread_create(&inc_x_thread, NULL, inc_x, &x)) {

fprintf(stderr, "Error creating thread\n");

return 1;

}

/* increment y to 100 in the first thread */

while(++y < 100);

printf("y increment finished\n");

/* wait for the second thread to finish */

if(pthread_join(inc_x_thread, NULL)) {

fprintf(stderr, "Error joining thread\n");

return 2;

}

/* show the results - x is now 100 thanks to the second thread */

printf("x: %d, y: %d\n", x, y);

return 0;

}

Command used to build:

-----------------------------------

/opt/poky/1.4.3/sysroots/i686-pokysdk-linux/usr/bin/armv7a-vfp-neon-poky-linux-gnueabi/arm-poky-linux-gnueabi-gcc -L/opt/fsl-imx6-sysroot/lib -L/opt/fsl-imx6-sysroot/usr/lib -lpthread test.c

0 件の賞賛
返信

7,663件の閲覧回数
LeonardoSandova
Specialist I

are you sourcing the environment script before compilation? the env script should be located somewhere on /opt/poky/<VERSION>/environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi

0 件の賞賛
返信

7,663件の閲覧回数
sumanranjan
Contributor III

Hi Leonardo,

I am getting this error too when I try to compile GStreamer Sample Application. I did source the environment script.I am able to compile and run a HelloWorld.c Application.

Sample application is from Chapter 10. Your first application link. The makefile I am using is attached below,

Makefile:

------------------------------------------------------------------------------------------------------------------------------------

# define the C compiler to use

CC = /opt/poky/1.4+snapshot/sysroots/i686-pokysdk-linux/usr/bin/cortexa9hf-vfp-neon-poky-linux-gnueabi/arm-poky-linux-gnueabi-gcc

# define any compile-time flags

CFLAGS = -Wall -g

# define any directories containing header files other than /usr/include

INCLUDES = -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/glib-2.0 -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/lib/glib-2.0/include/ -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/gstreamer-0.10/ -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/libxml2

LFLAGS = -L/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/lib

# define any libraries to link into executable:

LIBS = -lglib-2.0 -lxml2 -lgstreamer-0.10 -lgobject-2.0 -lz -lgmodule-2.0 -lffi

# define the C source files

SRCS = hellogst.c

# define the C object files

OBJS = $(SRCS:.c=.o)

# define the executable file

MAIN = hellogst

.PHONY: depend clean

all:    $(MAIN)

        @echo  Simple compiler named simple has been compiled

$(MAIN): $(OBJS)

        $(CC) $(CFLAGS) $(INCLUDES) -o $(MAIN) $(OBJS) $(LFLAGS) $(LIBS)

# this is a suffix replacement rule for building .o's from .c's

.c.o:

        $(CC) $(CFLAGS) $(INCLUDES) -c $<  -o $@

clean:

        $(RM) *.o *~ $(MAIN)

depend: $(SRCS)

        makedepend $(INCLUDES) $^

------------------------------------------------------------------------------------------------------------------------------------

Compilation Error:

------------------------------

$ make

/opt/poky/1.4+snapshot/sysroots/i686-pokysdk-linux/usr/bin/cortexa9hf-vfp-neon-poky-linux-gnueabi/arm-poky-linux-gnueabi-gcc -Wall -g -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/glib-2.0 -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/lib/glib-2.0/include/ -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/gstreamer-0.10/ -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/libxml2 -c hellogst.c  -o hellogst.o

/opt/poky/1.4+snapshot/sysroots/i686-pokysdk-linux/usr/bin/cortexa9hf-vfp-neon-poky-linux-gnueabi/arm-poky-linux-gnueabi-gcc -Wall -g -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/glib-2.0 -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/lib/glib-2.0/include/ -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/gstreamer-0.10/ -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/libxml2 -o hellogst hellogst.o -L/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/lib -lglib-2.0 -lxml2 -lgstreamer-0.10 -lgobject-2.0 -lz -lgmodule-2.0 -lffi

/opt/poky/1.4+snapshot/sysroots/i686-pokysdk-linux/usr/libexec/cortexa9hf-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.8.1/ld: cannot find /lib/libc.so.6

/opt/poky/1.4+snapshot/sysroots/i686-pokysdk-linux/usr/libexec/cortexa9hf-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.8.1/ld: cannot find /usr/lib/libc_nonshared.a

/opt/poky/1.4+snapshot/sysroots/i686-pokysdk-linux/usr/libexec/cortexa9hf-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.8.1/ld: cannot find /lib/ld-linux-armhf.so.3

collect2: error: ld returned 1 exit status

make: *** [hellogst] Error 1

0 件の賞賛
返信

7,663件の閲覧回数
sumanranjan
Contributor III

This issue has been resolved after manually editing the libpthread.so and libc.so file generated during yocto build. These files point to /usr/lib i.e. host pc libraries instead of current directory[/build-fb/tmp/sysroots/imx6qsabresd/usr/lib] which was causing the problem.

0 件の賞賛
返信

7,663件の閲覧回数
ieio
Contributor IV

Hi  Suman Ranjan,

what do u mean with "manualy editing libpthread.so and libc.so file"? Using an hex editor.

I am running exactly into your same problem.

What is strange is that I can successfully compile QT applications with qt creator following the instruction in  Setup QT Creator with Yocto Build

Thanks in advance,

i.

0 件の賞賛
返信

7,663件の閲覧回数
ieio
Contributor IV

Solved,

my problem was in the Makefile, pls refer to 5.2. of  Yocto Project Application Developer's Guide

CC and CFLAGS must be set properly.

i.

7,663件の閲覧回数
sumanranjan
Contributor III

You are right. I changed my CFLAGS accordingly and it worked too.

Makefile:

SYSROOT_PATH=/home/suman/svndump/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd

# define any compile-time flags

#CFLAGS  = -fPIC -Wall -Wextra -O2 -g  # old CFLAG

CFLAGS="--sysroot=$(SYSROOT_PATH)"  # New CFLAG fixes the problem