Yocto kernel compilation issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto kernel compilation issue

5,775 Views
veeranjaneyulug
Contributor III

we used kernel 3.14.28 and yocto .we run below commands

bitbake linux-imx -c compile -f

its compiled but when we gave build that time only itwill give dtb issue.

bitbake linux-imx -c build -f

|   CLEAN   scripts/genksyms

|   CLEAN   scripts/kconfig

|   CLEAN   scripts/mod

|   CLEAN   scripts

|   CLEAN   drivers/tty/vt

|   CLEAN   drivers/video/logo

| make: Leaving directory `/home/vishwa/workspace/veera_checkout_mar10/coderepo1/custom_mar11/tmp/work/imx6_zcam_custom-poky-linux-gnueabi/linux-imx/3.14.28-r0/image/usr/src/kernel'

| NOTE: make -j 4 imx6_zcam_custom.dtb

| make[1]: *** No rule to make target `arch/arm/boot/dts/imx6_zcam_custom.dtb'.  Stop.

| make: *** [imx6_zcam_custom.dtb] Error 2

| ERROR: oe_runmake failed

| WARNING: exit code 1 from a shell command.

| ERROR: Function failed: do_install (log file is located at /home/vishwa/workspace/veera_checkout_mar10/coderepo1/custom_mar11/tmp/work/imx6_zcam_custom-poky-linux-gnueabi/linux-imx/3.14.28-r0/temp/log.do_install.7621)

ERROR: Task 2 (/home/vishwa/workspace/veera_checkout_mar10/coderepo1/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.14.28.bb, do_install) failed with exit code '1'

NOTE: Tasks Summary: Attempted 407 tasks of which 402 didn't need to be rerun and 1 failed.

No currently running tasks (407 of 415)

Summary: 1 task failed:

  /home/vishwa/workspace/veera_chec

Labels (5)
0 Kudos
Reply
3 Replies

3,728 Views
shubhamsanghvi
Contributor II

Hello veeranjaneyulu g,

The 'compile' task builds only the zImage while the 'build' task will perform all the tasks for that specific recipe, 'linux-imx' in your case, which includes generating the dtb. So, Your dts is causing this build error. It looks like 'make' is not able to find the dts file  "imx6_zcam_custom.dts" in the arch/arm/boot/dts/ directory. Could you confirm that this file is present in the source or not?

Regards,

Shubham

0 Kudos
Reply

3,728 Views
veeranjaneyulug
Contributor III

Thanks for your reply.

yes that imx6_zcam_custom.dts is there in arch/arm/boot/dts directory .And Make file also i added imx6_zcam_custom.dtb line ..

0 Kudos
Reply

3,728 Views
jimmychan
NXP TechSupport
NXP TechSupport

have you add one line for your dtb in the makefile?

0 Kudos
Reply