Yocto imx8mpevk Intel Wifi Enabling

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Yocto imx8mpevk Intel Wifi Enabling

679 次查看
iamRoy
Contributor I

Hi,

I am using imx8m plus evk and Intel Corporation Wi-Fi 6 AX210 as WLAN card. Somehow, I cannot enable the Wifi.

root@imx8mpevk:~# uname -r
6.6.3-lts-next-gccf0a99701a7

root@imx8mpevk:~# lspci
00:00.0 PCI bridge: Synopsys, Inc. DWC_usb3 / PCIe bridge (rev 01)
01:00.0 Network controller: Intel Corporation Wi-Fi 6 AX210/AX211/AX411 160MHz (rev 1a)

root@imx8mpevk:~# ls -l /lib/firmware
-rw-r--r-- 1 root root 1499284 Jun 20 22:17 iwlwifi-ty-a0-gf-a0-72.ucode
-rw-r--r-- 1 root root 55020 Sep 20 15:19 iwlwifi-ty-a0-gf-a0.pnvm

root@imx8mpevk:~# sudo modprobe iwlwifi
modprobe: FATAL: Module iwlwifi not found in directory /lib/modules/6.6.3-lts-next-gccf0a99701a7

 

Furthermore, I am not able to download from the connected ethernet. I tried to search source.list but can't find anything.

root@imx8mpevk:~# ls /etc/apt/sources.list.d/
root@imx8mpevk:~#
root@imx8mpevk:~# ls /etc/apt/
apt.conf apt.conf.d auth.conf.d preferences.d sources.list.d trusted.gpg.d

root@imx8mpevk:~# apt-get install git
Reading package lists... Done
Building dependency tree... Done
E: Unable to locate package git

Is there any direction/guidance which I use to make the system working? I am not much familiar with the Yocto or NXP. I thorough guideline would be appreciated.

Thanks//Roy

0 项奖励
回复
3 回复数

647 次查看
iamRoy
Contributor I

Hi,

My target is to test the Intel wifi radio. Therefore, I must use the Intel Wi-Fi 6 AX210 card.

 

What about ethernet? Why can't I access repos/wget from the system? What configs should I take a look?

 

Thanks//Roy

0 项奖励
回复

601 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @iamRoy!

Unfortunatelly we can't  help you with the wifi drivers.

Sorry for the mistake!

 

Our BSP is not a Linux Distribution Like Debian or Ubuntu and to add packages to your rootfs should do it under Yocto Project.

 

Best Regards!

Chavira

0 项奖励
回复

660 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @iamRoy!

Thank you for contacting NXP Support!

 

Unfortunately, the device that you are using is not supported by our BSP.

To add support for that wifi should be under Yocto.

We recommend using our wifi devices because the drivers are integrated into our BSP and if you are using an EVK board you shouldn't have a problem using our wifi devices.

 

Sorry for the mistake!

 

Best Regards!

Chavira

0 项奖励
回复