Yocto error: Building libreoffice package fails in do_package task

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Yocto error: Building libreoffice package fails in do_package task

2,051 次查看
vladzouth
Contributor II

I would like to integrate libreoffice on my tx6s-8035 KARO Board using yocto. I use Ka-ro NXP/Freescale Yocto Project Community BSP recipe layers for yocto distro krogoth. I add too the meta-office layer from open-embedded. I have been facing many issues about packages and libraries dependency to build the libreoffice package. The do_compile task work well but the do_package task fails with the following error:

ERROR: libreoffice-5.0.6.3-r0 do_package: QA Issue: File  '/usr/lib/libreoffice/share/extensions/mysql-connector-  ooo/libmysqlclient_r.so' from libreoffice was already stripped, this will  prevent future debugging! [already-stripped] WARNING: libreoffice-5.0.6.3-r0 do_package: libreoffice language file  pattern not found:  /usr/lib/libreoffice/share/template/%{1} ERROR: libreoffice-5.0.6.3-r0 do_package: Fatal QA errors found, failing  task. ERROR: libreoffice-5.0.6.3-r0 do_package: Function failed: do_package ERROR: Logfile of failure stored in: /home/sconte/fsl-community-  bsp/build_8135_cim/tmp/work/cortexa9hf-neon-poky-linux-  gnueabi/libreoffice/5.0.6.3-r0/temp/log.do_package.8211 ERROR: Task 11 (/home/sconte/fsl-community-bsp/sources/meta-office/recipes-  libreoffice/libreoffice/libreoffice.bb, do_package) failed with exit code  '1'

Here is the log.do_package file output: log.do_package

I view in this file that there is runstrip function which is executed on the same library it cound not find. What does runstrip means? How can i work around this issue?

标签 (3)
0 项奖励
回复
1 回复

1,811 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Souleymane Conte,

I see that there is a suggested workaround on an external forum. I’d like to add a link here just for reference in case another community user stumbles upon a similar error:

https://stackoverflow.com/questions/49670136/yocto-error-building-libreoffice-package-fails-in-do-pa...

 

Regards,

0 项奖励
回复