Yocto doesn't support git binary diff - workaround?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto doesn't support git binary diff - workaround?

ソリューションへジャンプ
7,295件の閲覧回数
chris_f
Contributor V

I'm making minor modifications to my Yocto project using a layer that includes git patch files called up by bbappend files.

This was working fine until I tried to add a new logo BMP file which causes git to produce a binary diff.

This cause bitbake to fail with:

File tools/logos/mx6ullevk.bmp: git binary diffs are not supported.
Patch 0002-First-steps-at-a-useable-python-file-to-create-bitma.patch does not apply (enforce with -f)

That's a pain. Can someone suggest a simple work around?

Build Configuration:
BB_VERSION = "1.30.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-16.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6ull14x14evk"
DISTRO = "fsl-imx-fb"
DISTRO_VERSION = "4.1.15-2.0.1"

ラベル(2)
タグ(1)
1 解決策
6,450件の閲覧回数
chris_f
Contributor V

I worked around the problem by storing my new bmp in base64 encoded format and using the Makefile to produce the binary. It's not nice but it works.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
6,451件の閲覧回数
chris_f
Contributor V

I worked around the problem by storing my new bmp in base64 encoded format and using the Makefile to produce the binary. It's not nice but it works.

0 件の賞賛
返信