Yocto compilation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto compilation

2,668件の閲覧回数
sergio_dorazio
Contributor IV

Hi,

I am using yocto project for compile my linux on IMX6ULL EVK.

I am starting from Image 'core-image-base' and I am adding some modules with command IMAGE_INSTALL_append =  "lighttpd curl libstdc++ bluez5" in local.conf file.
I build with bitbake command and I have a file system with new modules.

But when I run these mudules there are errors: some library file not found because the folder 'modules' in '~/imx-yocto-bsp/Linux-RCA2/tmp/deploy/images/imx6ull14x14evk'  is not update with new modules, infact the date of this folder is old.

What is the command for update this folder ?

By.

Sergio.

0 件の賞賛
返信
5 返答(返信)

2,502件の閲覧回数
sergio_dorazio
Contributor IV

Hi Romit,

thankyou for answer , but with your commands the forder

-  "~/imx-yocto-bsp/Linux-RCA2/tmp/deploy/images/imx6ull14x14evk/modules",

the files

-  "~/imx-yocto-bsp/Linux-RCA2/tmp/deploy/images/imx6ull14x14evk/modules--4.14.98-r0-imx6ull14x14evk-20190701130715.tgz"

and

-  "~/imx-yocto-bsp/Linux-RCA2/tmp/deploy/images/imx6ull14x14evk/modules--4.14.98-r0-imx6ull14x14evk-20190701130715.tgz"

are not update !!!!!!!!!!!!!!!!

Seems this files and folder are create only when install at first time yocto project !!!!

Have you other help for me ?

Sergio.

0 件の賞賛
返信

2,502件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Sergio,

The cleanall command should clean up the entirety of the downloaded sources and compiled binaries, which would force everything to be build again.

I hope this helps!

Regards,

0 件の賞賛
返信

2,502件の閲覧回数
romitchatterjee
Contributor V

You can always brute force build everything by deleting the tmp/, cache/ and sstate-cache/ folders and rebuilding. Not a very good solution though, it builds everything from scratch again.

2,502件の閲覧回数
romitchatterjee
Contributor V

Try cleaning and rebuilding, and see if that helps:

bitbake -c clean core-image-base

bitbake -c cleansstate core-image-base

bitbake core-image-base

0 件の賞賛
返信

2,502件の閲覧回数
sergio_dorazio
Contributor IV

The library files not found are for example : mod_proxy.so, mod_status.so, .....

0 件の賞賛
返信