Yocto build. ERROR: onnxruntime-1.8.2-r0 do_package_qa: QA run found fatal errors. 5.10.72-2.2.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto build. ERROR: onnxruntime-1.8.2-r0 do_package_qa: QA run found fatal errors. 5.10.72-2.2.0

4,724件の閲覧回数
WilliamBagshaw-imd
Contributor II

I am using a BSP build "as is" and getting an error...


ERROR: onnxruntime-1.8.2-r0 do_package_qa: QA Issue: /usr/lib/python3.9/site-packages/bin/onnxruntime_test contained in package onnxruntime requires /short2/bld-xwayland/tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.8.2-r0/recipe-sysroot-native/usr/bin/nativepython3, but no providers found in RDEPENDS_onnxruntime? [file-rdeps]
ERROR: onnxruntime-1.8.2-r0 do_package_qa: QA run found fatal errors. Please consider fixing them.
ERROR: Logfile of failure stored in: /short2/bld-xwayland/tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.8.2-r0/temp/log.do_package_qa.2763304
ERROR: Task (/short2/sources/meta-imx/meta-ml/recipes-libraries/onnxruntime/onnxruntime_1.8.2.bb:do_package_qa) failed with exit code '1'

 

The commands I am executing are...

repo init -u git@github.com:nxp-imx/imx-manifest.git -b imx-linux-hardknott -m imx-5.10.72-2.2.0.xml
repo sync
DISTRO=fsl-imx-xwayland MACHINE=imx8mpevk  source ./imx-setup-release.sh -b bld-xwayland
bitbake onnxruntime

This looks like a similar issue but the recipe references a different repository.
https://community.nxp.com/t5/i-MX-Processors/Yocto-imx-image-full-build-error-with-onnxruntime-qa-is...

The recipe that I am using references...

ONNXRUNTIME_SRC ?= "gitsm://github.com/nxp-imx/onnxruntime-imx.git;protocol=https"
SRCBRANCH = "lf-5.10.72_2.2.0"

SRCREV = "d5d8898338f8713d09ff0e85b6ddbe464138baf7"




ラベル(3)
0 件の賞賛
返信
8 返答(返信)

4,605件の閲覧回数
WilliamBagshaw-imd
Contributor II

Work around.

I could not identify why the onnxruntime package does not build reliably. It would sometimes work when building a full image.

However, it seamed to reliably build only when using pre downloaded files, and then completely rebuilding the full image. Rebuilding the full image, including downloading, is unreliable.

0 件の賞賛
返信

4,668件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @WilliamBagshaw-imd,

Please use the following NXP iMX Repo Manifest and restart the build process.

GitHub - nxp-imx/imx-manifest at imx-linux-hardknott

To download the 5.10.72-2.2.2 release
repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-hardknott -m imx-5.10.72-2.2.2.xml

Note: The remaining instructions are for setting up a BSP release only. For setting
up a demo, please see imx-manifest/README-<demo> for further instructions.

$: [MACHINE=<machine>] [DISTRO=fsl-imx-<backend>] source ./imx-setup-release.sh -b bld-<backend>

<machine> defaults to imx6qsabresd

<backend> Graphics backend type
xwayland Wayland with X11 support - default distro
wayland Wayland
fb Framebuffer (not supported for mx8)

Note if the poky community distro is used then build breaks will happen with some
components using our meta-imx layer.

 I hope this information will be helpful. 

Have a great day!

0 件の賞賛
返信

4,660件の閲覧回数
WilliamBagshaw-imd
Contributor II

I have been using the following commands repeatedly in different empty directories.
repo init -u git@github.com:nxp-imx/imx-manifest.git -b imx-linux-hardknott -m imx-5.10.72-2.2.0.xml

repo sync
DISTRO=fsl-imx-xwayland MACHINE=imx8mpevk  source ./imx-setup-release.sh -b bld-xwayland
bitbake onnxruntime

I get the same error.

0 件の賞賛
返信

4,654件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @WilliamBagshaw-imd,

Thank you for your reply.

Could you please help me to understand what you are building only the onnxruntime package?

This package depends on other packages to correctly implement machine learning.

Please try with the command bitbake imx-image-full, this command will build all the packages required for multimedia and machine learning. 

Best regards, Brian.

0 件の賞賛
返信

4,644件の閲覧回数
WilliamBagshaw-imd
Contributor II

This is the "minimal reproducible example". Bitbake will automatically build all dependencies. (unless there is an issue.) I can try the full image this will take a long time to build. I have had this issue with full images. That is why I simplified the problem to just being unable to build one package.

0 件の賞賛
返信

4,642件の閲覧回数
WilliamBagshaw-imd
Contributor II

This morning the full image built fine.

repo init -u git@github.com:nxp-imx/imx-manifest.git -b imx-linux-hardknott -m imx-5.10.72-2.2.0.xml
repo sync
DISTRO=fsl-imx-xwayland MACHINE=imx8mpevk  source ./imx-setup-release.sh -b bld-xwayland
bitbake imx-image-full

Can you explain why this is? I have had full images sometimes work and sometimes fail. Building of just the package should work. If there is a package that is needed by onnxruntime the package should be dependent on it. It appears to be luck as to if the full image builds in the correct order.
0 件の賞賛
返信

4,634件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @WilliamBagshaw-imd,

Thank you for your update. 

And yes, as I said before the onnxruntime is part of machine learning package and depends on other packages to correctly build. 

Have a great day! 

0 件の賞賛
返信

4,606件の閲覧回数
WilliamBagshaw-imd
Contributor II

This is not an explanation. Dependences are supposed to be handles by bitbake. The recipe should contain those dependencies.

0 件の賞賛
返信