Yocto U-Boot Port for Custom Device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto U-Boot Port for Custom Device

ソリューションへジャンプ
1,608件の閲覧回数
PaulDeMetrotion
Senior Contributor I

I am attempting to move from LTIB to Yocto on a custom i.MX6 SBC. I cannot get u-boot to work yet. I started with the Sabre-SD files and added the customization from the LTIB files that have already been verified. I believe I have two issues:

1. I cannot get anything to display to the console before the MMC line. I would expect to see some text before the first line. I have included a checkboard() function that should output the board name at least. Can't seem to add any debug puts instructions to help. Don't even know if this function is being executed. Here is the console output:

MMC:   FSL_SDHC: 0, FSL_SDHC: 1

sd_send_op_cond()

sd_send_op_cond() - 1

Card did not respond to voltage select!

MMC init failed

Using default environment

2. MMC device is failing. As can be seen the MMC initialization has failed. Have not really looked at this yet since I have been focusing on issue 1. Any insights would be appreciated.

I can provide more information if required. Thanks in advance.

ラベル(2)
0 件の賞賛
返信
1 解決策
1,451件の閲覧回数
PaulDeMetrotion
Senior Contributor I

I have resolved these issues.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,452件の閲覧回数
PaulDeMetrotion
Senior Contributor I

I have resolved these issues.

0 件の賞賛
返信