Yocto Standard SDK vs Extensible SDK: What is the difference ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto Standard SDK vs Extensible SDK: What is the difference ?

ソリューションへジャンプ
4,726件の閲覧回数
khang_letruong
Senior Contributor III

Dear Yocto Experts,

I learnt about Yocto Extensible SDK from following discussion : https://community.nxp.com/t5/i-MX-Processors/Yocto-Hardknott-and-iMX8MP-error-generating-extended-sd...

I would like to know what is the difference if any.

Thanks in advance and best regards,

Khang

0 件の賞賛
返信
1 解決策
4,688件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

As per Yocto eSDK Manual:

The extensible SDK provides a cross-development toolchain and libraries tailored to the contents of a specific image. You would use the Extensible SDK if you want a toolchain experience supplemented with the powerful set of devtool commands tailored for the Yocto Project environment.

The installed extensible SDK consists of several files and directories. Basically, it contains an SDK environment setup script, some configuration files, an internal build system, and the devtool functionality.

As you can see in Yocto eSDK Manual and Toradex Community, devtool is the main feature of it.

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,689件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

As per Yocto eSDK Manual:

The extensible SDK provides a cross-development toolchain and libraries tailored to the contents of a specific image. You would use the Extensible SDK if you want a toolchain experience supplemented with the powerful set of devtool commands tailored for the Yocto Project environment.

The installed extensible SDK consists of several files and directories. Basically, it contains an SDK environment setup script, some configuration files, an internal build system, and the devtool functionality.

As you can see in Yocto eSDK Manual and Toradex Community, devtool is the main feature of it.

Regards

0 件の賞賛
返信