Yocto PCI Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto PCI Error

Jump to solution
8,366 Views
kikimorisato
Contributor II

BSP: fsl-community-bsp (fido branch)

Kernel Version: 3.14.28

Board: SabreSD (mx6q)

Kernel Config

Bus support -> [*] PCI support

   PCI host controller drivers -> [*] Freescale i.MX6 PCIe contoroller

i did not check extremely power save mode / EP / RC / Generic PCI host controller

-------------------------------------------------------------------------------

but PCI irq error

LTIB (L3.0.35_4.1.0_138016 has no problem)

-------------------------------------------------------------------------------


plz help me!!!


here is my console message


-------------------------------------------------------------------------------

U-Boot 2015.04-rc5+fslc+gc0e89c7 (Apr 15 2015 - 10:28:10)

CPU:   Freescale i.MX6Q rev1.5 at 792 MHz

CPU:   Temperature 30 C

Reset cause: POR

Board: MX6-SabreSD

I2C:   ready

DRAM:  1 GiB

PMIC:  PFUZE100 ID=0x10

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

  00:01.0     - 16c3:abcd - Bridge device

   01:00.0    - 1797:6869 - Build before PCI Rev2.0

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:   serial

Err:   serial

Net:   Phy 1 not found

PHY reset timed out

FEC [PRIME]

Error: FEC address not set.

Hit any key to stop autoboot:  0

switch to partitions #0, OK

mmc1 is current device

reading boot.scr

** Unable to read file boot.scr **

reading zImage

6072280 bytes read in 315 ms (18.4 MiB/s)

Booting from mmc ...

reading imx6q-sabresd-ldo.dtb

42219 bytes read in 25 ms (1.6 MiB/s)

Kernel image @ 0x12000000 [ 0x000000 - 0x5ca7d8 ]

## Flattened Device Tree blob at 18000000

   Booting using the fdt blob at 0x18000000

   Using Device Tree in place at 18000000, end 1800d4ea

Starting kernel ...

Booting Linux on physical CPU 0x0

Linux version 3.14.28-1.0.0_ga+g91cf351 (kimjh@kimjh-virtual-machine) (gcc version 4.9.2 (GCC) ) #1 SMP PREEMPT Mon Apr 20 13:55:04 KST 2015

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine model: Freescale i.MX6 Quad Sane Board

cma: CMA: reserved 320 MiB at 3c000000

Memory policy: Data cache writealloc

PERCPU: Embedded 8 pages/cpu @ab723000 s8896 r8192 d15680 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260096

Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=ldb,1024x600M@60,if=RGB666

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 696176K/1048576K available (7371K kernel code, 398K rwdata, 6260K rodata, 336K init, 429K bss, 352400K reserved, 0K highmem)

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    vmalloc : 0xc0800000 - 0xff000000   (1000 MB)

    lowmem  : 0x80000000 - 0xc0000000   (1024 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .text : 0x80008000 - 0x80d57e1c   (13632 kB)

      .init : 0x80d58000 - 0x80dac2c0   ( 337 kB)

      .data : 0x80dae000 - 0x80e118e0   ( 399 kB)

       .bss : 0x80e118ec - 0x80e7d05c   ( 430 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1

Preemptible hierarchical RCU implementation.

NR_IRQS:16 nr_irqs:16 16

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1024 kB

Switching to timer-based delay loop

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns

Console: colour dummy device 80x30

Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)

Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x10703b68 - 0x10703bc0

CPU1: Booted secondary processor

CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

CPU2: Booted secondary processor

CPU2: thread -1, cpu 2, socket 0, mpidr 80000002

CPU3: Booted secondary processor

CPU3: thread -1, cpu 3, socket 0, mpidr 80000003

Brought up 4 CPUs

SMP: Total of 4 processors activated.

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

pinctrl core: initialized pinctrl subsystem

regulator-dummy: no parameters

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

cpuidle: using governor ladder

cpuidle: using governor menu

CPU identified as i.MX6Q, silicon rev 1.5

Use WDOG1 as reset source

syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered

vdd1p1: 800 <--> 1375 mV at 1100 mV

vdd3p0: 2800 <--> 3150 mV at 3000 mV

vdd2p5: 2000 <--> 2750 mV at 2400 mV

vddarm: 725 <--> 1450 mV at 1150 mV

vddpu: 725 <--> 1450 mV at 1150 mV

vddsoc: 725 <--> 1450 mV at 1175 mV

syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered

syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

bio: create slab <bio-0> at 0

mxs-dma 110000.dma-apbh: initialized

usb_otg_vbus: 5000 mV

usb_h1_vbus: 5000 mV

wm8962-supply: no parameters

mipi_dsi_pwr_on: no parameters

sensor-supply: 3300 mV

vgaarb: loaded

i2c-core: driver [max17135] using legacy suspend method

i2c-core: driver [max17135] using legacy resume method

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

usbphy_nop1.12 supply vcc not found, using dummy regulator

usbphy_nop2.13 supply vcc not found, using dummy regulator

i2c i2c-0: IMX I2C adapter registered

i2c i2c-1: IMX I2C adapter registered

i2c i2c-2: IMX I2C adapter registered

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>

PTP clock support registered

imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed

mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Initialized.

Bluetooth: Core ver 2.18

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

cfg80211: Calling CRDA to update world regulatory domain

Switched to clocksource mxc_timer1

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 3, 32768 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

TCP: reno registered

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

imx6_busfreq busfreq.16: DDR medium rate not supported.

Bus freq driver module loaded

futex hash table entries: 1024 (order: 4, 65536 bytes)

VFS: Disk quotas dquot_6.5.2

Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

jffs2: version 2.2. (NAND) ⓒ 2001-2006 Red Hat, Inc.

fuse init (API version 7.22)

msgmni has been set to 1999

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

imx-weim 21b8000.weim: Driver registered.

imx6q-pcie 1ffc000.pcie: PCI host bridge to bus 0000:00

pci_bus 0000:00: root bus resource [io  0x1000-0x10000]

pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]

pci_bus 0000:00: root bus resource [bus 00-ff]

PCI: bus0: Fast back to back transfers disabled

pci 0000:01:00.0: Setting PCI class for tw6865 PCIe device

PCI: bus1: Fast back to back transfers disabled

pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]

pci 0000:00:00.0: BAR 9: assigned [mem 0x01100000-0x011fffff pref]

pci 0000:00:00.0: BAR 6: assigned [mem 0x01200000-0x0120ffff pref]

pci 0000:01:00.0: BAR 0: assigned [mem 0x01100000-0x01100fff pref]

pci 0000:00:00.0: PCI bridge to [bus 01]

pci 0000:00:00.0:   bridge window [mem 0x01100000-0x011fffff pref]

------------[ cut here ]------------

WARNING: CPU: 0 PID: 1 at /home/kimjh/fsl-community-bsp/build/tmp/work-shared/imx6qsabresd/kernel-source/kernel/irq/manage.c:1412 request_threaded_irq+0xfc/0x124()

Modules linked in:

CPU: 0 PID: 1 Comm: swapper/0 Not tainted 3.14.28-1.0.0_ga+g91cf351 #1

[<800155f0>] (unwind_backtrace) from [<800116d4>] (show_stack+0x10/0x14)

[<800116d4>] (show_stack) from [<806fd950>] (dump_stack+0x7c/0xbc)

[<806fd950>] (dump_stack) from [<8002d6d8>] (warn_slowpath_common+0x70/0x8c)

[<8002d6d8>] (warn_slowpath_common) from [<8002d790>] (warn_slowpath_null+0x1c/0x24)

[<8002d790>] (warn_slowpath_null) from [<80069cec>] (request_threaded_irq+0xfc/0x124)

[<80069cec>] (request_threaded_irq) from [<802c94f4>] (pcie_pme_probe+0x98/0x1b4)

[<802c94f4>] (pcie_pme_probe) from [<802c8720>] (pcie_port_probe_service+0x38/0x84)

[<802c8720>] (pcie_port_probe_service) from [<8034dd20>] (driver_probe_device+0x110/0x24c)

[<8034dd20>] (driver_probe_device) from [<8034c324>] (bus_for_each_drv+0x64/0x98)

[<8034c324>] (bus_for_each_drv) from [<8034dbe0>] (device_attach+0x74/0x88)

[<8034dbe0>] (device_attach) from [<8034d264>] (bus_probe_device+0x84/0xa8)

[<8034d264>] (bus_probe_device) from [<8034b6e0>] (device_add+0x450/0x538)

[<8034b6e0>] (device_add) from [<802c89fc>] (pcie_port_device_register+0x1f8/0x230)

[<802c89fc>] (pcie_port_device_register) from [<802c8cc4>] (pcie_portdrv_probe+0x3c/0xa4)

[<802c8cc4>] (pcie_portdrv_probe) from [<802bfbf8>] (pci_device_probe+0x74/0xc8)

[<802bfbf8>] (pci_device_probe) from [<8034dd20>] (driver_probe_device+0x110/0x24c)

[<8034dd20>] (driver_probe_device) from [<8034c324>] (bus_for_each_drv+0x64/0x98)

[<8034c324>] (bus_for_each_drv) from [<8034dbe0>] (device_attach+0x74/0x88)

[<8034dbe0>] (device_attach) from [<802b80cc>] (pci_bus_add_device+0x34/0x64)

[<802b80cc>] (pci_bus_add_device) from [<802b81e4>] (pci_bus_add_devices+0x3c/0xa0)

[<802b81e4>] (pci_bus_add_devices) from [<800137b8>] (pci_common_init_dev+0x224/0x2ec)

[<800137b8>] (pci_common_init_dev) from [<80d82c14>] (dw_pcie_host_init+0x640/0x670)

[<80d82c14>] (dw_pcie_host_init) from [<80d82f3c>] (imx6_pcie_probe+0x2e4/0x328)

[<80d82f3c>] (imx6_pcie_probe) from [<8034f494>] (platform_drv_probe+0x44/0xa4)

[<8034f494>] (platform_drv_probe) from [<8034dd20>] (driver_probe_device+0x110/0x24c)

[<8034dd20>] (driver_probe_device) from [<8034df2c>] (__driver_attach+0x8c/0x90)

[<8034df2c>] (__driver_attach) from [<8034c278>] (bus_for_each_dev+0x6c/0xa0)

[<8034c278>] (bus_for_each_dev) from [<8034d4d8>] (bus_add_driver+0x148/0x1f0)

[<8034d4d8>] (bus_add_driver) from [<8034e528>] (driver_register+0x78/0xf8)

[<8034e528>] (driver_register) from [<8034f51c>] (platform_driver_probe+0x20/0xa8)

[<8034f51c>] (platform_driver_probe) from [<8000889c>] (do_one_initcall+0xf8/0x154)

[<8000889c>] (do_one_initcall) from [<80d58c54>] (kernel_init_freeable+0x138/0x1d8)

[<80d58c54>] (kernel_init_freeable) from [<806f9038>] (kernel_init+0x8/0xe8)

[<806f9038>] (kernel_init) from [<8000e4f8>] (ret_from_fork+0x14/0x3c)

---[ end trace 1e0f8522328b0baa ]---

pcie_pme: probe of 0000:00:00.0:pcie01 failed with error -22

backlight.29 supply power not found, using dummy regulator

mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed

MIPI DSI driver module loaded

mxc_sdc_fb fb.24: registered mxc display driver ldb

imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

Console: switching to colour frame buffer device 128x48

mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1

fbcvt: 1920x1080@60: CVT Name - 2.073M9

mxc_sdc_fb fb.25: registered mxc display driver hdmi

mxc_sdc_fb fb.26: registered mxc display driver lcd

mxc_sdc_fb fb.26: ipu0-di0 already in use

mxc_sdc_fb: probe of fb.26 failed with error -16

mxc_sdc_fb fb.27: registered mxc display driver ldb

imx-sdma 20ec000.sdma: no iram assigned, using external mem

imx-sdma 20ec000.sdma: no event needs to be remapped

imx-sdma 20ec000.sdma: loaded firmware 3.1

imx-sdma 20ec000.sdma: initialized

pfuze100-regulator 1-0008: Full layer: 1, Metal layer: 1

pfuze100-regulator 1-0008: FAB: 0, FIN: 0

pfuze100-regulator 1-0008: pfuze100 found.

SW1AB: 300 <--> 1875 mV at 1375 mV

SW1C: 300 <--> 1875 mV at 1375 mV

SW2: 800 <--> 3300 mV at 3300 mV

SW3A: 400 <--> 1975 mV at 1500 mV

SW3B: 400 <--> 1975 mV at 1500 mV

SW4: 800 <--> 3300 mV at 3150 mV

SWBST: 5000 <--> 5150 mV at 5000 mV

VSNVS: 1000 <--> 3000 mV at 3000 mV

VREFDDR: 750 mV

VGEN1: 800 <--> 1550 mV at 1500 mV

VGEN2: 800 <--> 1550 mV at 1500 mV

VGEN3: 1800 <--> 3300 mV at 2800 mV

VGEN4: 1800 <--> 3300 mV at 1800 mV

VGEN5: 1800 <--> 3300 mV at 3000 mV

VGEN6: 1800 <--> 3300 mV at 3300 mV

Serial: IMX driver

2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58, base_baud = 5000000) is a IMX

console [ttymxc0] enabled

serial: Freescale lpuart driver

imx sema4 driver is registered.

[drm] Initialized drm 1.1.0 20060810

[drm] Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

loop: module loaded

ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024

ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480

ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000

ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000

ahci-imx 2200000.sata: failed to reset phy: -110

ahci-imx: probe of 2200000.sata failed with error -110

m25p80 spi0.0: found mr25h256, expected m25p32

m25p80 spi0.0: mr25h256 (32 Kbytes)

spi_imx 2008000.ecspi: probed

CAN device driver interface

2188000.ethernet supply phy not found, using dummy regulator

pps pps0: new PPS source ptp0

fec 2188000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00

fec 2188000.ethernet (unregistered net_device): Using random MAC address: 5a:bf:06:68:f9:63

libphy: fec_enet_mii_bus: probed

fec 2188000.ethernet eth0: registered PHC device 0

usbcore: registered new interface driver asix

usbcore: registered new interface driver cdc_ether

usbcore: registered new interface driver cdc_ncm

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-pci: EHCI PCI platform driver

ehci-mxc: Freescale On-Chip EHCI Host driver

usbcore: registered new interface driver usb-storage

2184800.usbmisc supply vbus-wakeup not found, using dummy regulator

ci_hdrc ci_hdrc.0: EHCI Host Controller

ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

ci_hdrc ci_hdrc.1: doesn't support gadget

ci_hdrc ci_hdrc.1: EHCI Host Controller

ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2

ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

mousedev: PS/2 mouse device common for all mice

egalax_ts 1-0004: Failed to read firmware version

egalax_ts: probe of 1-0004 failed with error -5

egalax_ts 2-0004: Failed to read firmware version

egalax_ts: probe of 2-0004 failed with error -5

input: max11801_ts as /devices/soc0/soc.0/2100000.aips-bus/21a4000.i2c/i2c-1/1-0048/input/input2

i2c-core: driver [isl29023] using legacy suspend method

i2c-core: driver [isl29023] using legacy resume method

snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0

i2c /dev entries driver

IR NEC protocol handler initialized

IR RC5(x) protocol handler initialized

IR RC6 protocol handler initialized

IR JVC protocol handler initialized

IR Sony protocol handler initialized

IR RC5 (streamzap) protocol handler initialized

IR SANYO protocol handler initialized

IR MCE Keyboard/mouse protocol handler initialized

mxc_v4l2_output v4l2_out.32: V4L2 device registered as video16

mxc_v4l2_output v4l2_out.32: V4L2 device registered as video17

mxc_v4l2_output v4l2_out.32: V4L2 device registered as video18

mxc_v4l2_output v4l2_out.32: V4L2 device registered as video19

mxc_v4l2_output v4l2_out.32: V4L2 device registered as video20

PCI: enabling device 0000:01:00.0 (0140 -> 0142)

------------[ cut here ]------------

WARNING: CPU: 0 PID: 1 at /home/kimjh/fsl-community-bsp/build/tmp/work-shared/imx6qsabresd/kernel-source/kernel/irq/manage.c:1412 request_threaded_irq+0xfc/0x124()

Modules linked in:

CPU: 0 PID: 1 Comm: swapper/0 Tainted: G        W    3.14.28-1.0.0_ga+g91cf351 #1

[<800155f0>] (unwind_backtrace) from [<800116d4>] (show_stack+0x10/0x14)

[<800116d4>] (show_stack) from [<806fd950>] (dump_stack+0x7c/0xbc)

[<806fd950>] (dump_stack) from [<8002d6d8>] (warn_slowpath_common+0x70/0x8c)

[<8002d6d8>] (warn_slowpath_common) from [<8002d790>] (warn_slowpath_null+0x1c/0x24)

[<8002d790>] (warn_slowpath_null) from [<80069cec>] (request_threaded_irq+0xfc/0x124)

[<80069cec>] (request_threaded_irq) from [<8006b800>] (devm_request_threaded_irq+0x58/0x9c)

[<8006b800>] (devm_request_threaded_irq) from [<804a0008>] (tw6869_probe+0x324/0x878)

[<804a0008>] (tw6869_probe) from [<802bfbf8>] (pci_device_probe+0x74/0xc8)

[<802bfbf8>] (pci_device_probe) from [<8034dd20>] (driver_probe_device+0x110/0x24c)

[<8034dd20>] (driver_probe_device) from [<8034df2c>] (__driver_attach+0x8c/0x90)

[<8034df2c>] (__driver_attach) from [<8034c278>] (bus_for_each_dev+0x6c/0xa0)

[<8034c278>] (bus_for_each_dev) from [<8034d4d8>] (bus_add_driver+0x148/0x1f0)

[<8034d4d8>] (bus_add_driver) from [<8034e528>] (driver_register+0x78/0xf8)

[<8034e528>] (driver_register) from [<8000889c>] (do_one_initcall+0xf8/0x154)

[<8000889c>] (do_one_initcall) from [<80d58c54>] (kernel_init_freeable+0x138/0x1d8)

[<80d58c54>] (kernel_init_freeable) from [<806f9038>] (kernel_init+0x8/0xe8)

[<806f9038>] (kernel_init) from [<8000e4f8>] (ret_from_fork+0x14/0x3c)

---[ end trace 1e0f8522328b0bab ]---

tw6869 0000:01:00.0: request_irq failed

tw6869: probe of 0000:01:00.0 failed with error -22

usb 1-1: new high-speed USB device number 2 using ci_hdrc

mag3110 2-000e: check mag3110 chip ID

mag3110 2-000e: read chip ID 0xfffffffb is not equal to 0xc4!

mag3110: probe of 2-000e failed with error -22

i2c-core: driver [mag3110] using legacy suspend method

i2c-core: driver [mag3110] using legacy resume method

mma8451 0-001c: read chip ID 0x1 is not equal to 0x1a or 0x2a!

mma8451: probe of 0-001c failed with error -22

imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCI H4 protocol initialized

Bluetooth: HCI BCSP protocol initialized

Bluetooth: HCIATH3K protocol initialized

usbcore: registered new interface driver bcm203x

usbcore: registered new interface driver btusb

Bluetooth: Generic Bluetooth SDIO driver ver 0.1

usbcore: registered new interface driver ath3k

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

hub 1-1:1.0: USB hub found

mmc1: no vqmmc regulator found

mmc1: no vmmc regulator found

hub 1-1:1.0: 4 ports detected

mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA

mmc2: no vqmmc regulator found

mmc2: no vmmc regulator found

mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA

mmc3: no vqmmc regulator found

mmc3: no vmmc regulator found

mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA

Galcore version 5.0.11.25762

mmc2: new high speed SDHC card at address b368

mmcblk2: mmc2:b368 SDC   7.45 GiB

mmcblk2: p1 p2

mmc3: BKOPS_EN bit is not set

mmc3: new high speed DDR MMC card at address 0001

mmcblk3: mmc3:0001 M8G2FA 7.45 GiB

mmcblk3boot0: mmc3:0001 M8G2FA partition 1 512 KiB

mmcblk3boot1: mmc3:0001 M8G2FA partition 2 512 KiB

mmcblk3rpmb: mmc3:0001 M8G2FA partition 3 128 KiB

usb 1-1.2: new high-speed USB device number 3 using ci_hdrc

mmcblk3: p1

mmcblk3boot1: unknown partition table

mmcblk3boot0: unknown partition table

mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

mxc_vpu 2040000.vpu: VPU initialized

caam 2100000.caam: Instantiated RNG4 SH0

asix 1-1.2:1.0 eth1: register 'asix' at usb-ci_hdrc.0-1.2, ASIX AX88772 USB 2.0 Ethernet, 00:1e:c2:ff:7f:16

caam 2100000.caam: Instantiated RNG4 SH1

caam 2100000.caam: device ID = 0x0a160100 (Era 4)

caam 2100000.caam: job rings = 2, qi = 0

caam algorithms registered in /proc/crypto

caam_jr 2101000.jr0: registering rng-caam

platform caam_sm: blkkey_ex: 4 keystore units available

platform caam_sm: 64-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: 64-bit black key:

platform caam_sm: [0000] 5e 22 7a bc 33 d1 00 81

platform caam_sm: [0008] a7 89 06 d9 d9 94 27 d2

platform caam_sm: 128-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f

platform caam_sm: 128-bit black key:

platform caam_sm: [0000] d8 3f 70 49 83 1f 78 92

platform caam_sm: [0008] b5 45 fe f4 a2 96 15 5d

platform caam_sm: 192-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f

platform caam_sm: [0016] 10 11 12 13 14 15 16 17

platform caam_sm: 192-bit black key:

platform caam_sm: [0000] c1 4a 58 87 91 b7 ce a2

platform caam_sm: [0008] 36 75 ba 23 76 92 a9 46

platform caam_sm: [0016] f9 7e cb 45 4c 87 0f 4b

platform caam_sm: [0024] a1 db 20 ff 75 08 6f dc

platform caam_sm: 256-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f

platform caam_sm: [0016] 10 11 12 13 14 15 16 17

platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f

platform caam_sm: 256-bit black key:

platform caam_sm: [0000] 61 c9 9e d4 9c 03 64 79

platform caam_sm: [0008] 80 4a bf 01 d8 4a 8c 5d

platform caam_sm: [0016] 27 96 b1 88 6b c5 fa e6

platform caam_sm: [0024] 18 b0 26 96 a4 6e 02 28

platform caam_sm: 64-bit unwritten blob:

platform caam_sm: [0000] 00 00 00 00 00 00 00 00

platform caam_sm: [0008] 00 00 00 00 00 00 00 00

platform caam_sm: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform caam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 128-bit unwritten blob:

platform caam_sm: [0000] 00 00 00 00 00 00 00 00

platform caam_sm: [0008] 00 00 00 00 00 00 00 00

platform caam_sm: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform caam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 196-bit unwritten blob:

platform caam_sm: [0000] 00 00 00 00 00 00 00 00

platform caam_sm: [0008] 00 00 00 00 00 00 00 00

platform caam_sm: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform caam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 256-bit unwritten blob:

platform caam_sm: [0000] 00 00 00 00 00 00 00 00

platform caam_sm: [0008] 00 00 00 00 00 00 00 00

platform caam_sm: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform caam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 64-bit black key in blob:

platform caam_sm: [0000] 04 3e 69 ae db 73 76 e2

platform caam_sm: [0008] a4 25 69 3e 7e 90 ad 6a

platform caam_sm: [0016] f3 8d 3d 2d 91 7c 6b 80

platform caam_sm: [0024] 0a be ba ce 5e 21 83 62

platform caam_sm: [0032] e4 b3 be 69 92 78 b0 d3

platform caam_sm: [0040] 97 b8 83 a6 90 e5 58 ee

platform caam_sm: [0048] ed 69 4a 2d 5f 7c cc 2e

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 128-bit black key in blob:

platform caam_sm: [0000] b6 a9 7a 07 6b db 55 d2

platform caam_sm: [0008] 7c e3 ba cf 46 44 ad b3

platform caam_sm: [0016] 4c 49 4e c9 de fc 88 38

platform caam_sm: [0024] 87 6e 54 1b 6a 92 4c 55

platform caam_sm: [0032] ae 21 2c d6 eb ec 3c 57

platform caam_sm: [0040] 76 73 99 24 49 e0 09 47

platform caam_sm: [0048] 46 17 be 53 0e c2 93 fb

platform caam_sm: [0056] 32 82 0c fe fc 10 59 86

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 192-bit black key in blob:

platform caam_sm: [0000] 65 22 3f b0 0a 50 be 5c

platform caam_sm: [0008] af 1b 02 66 1e df 7d d5

platform caam_sm: [0016] c9 0f 45 84 4f f1 9b e3

platform caam_sm: [0024] 00 39 9f 37 8c 4e 17 56

platform caam_sm: [0032] 83 ed 3b 61 21 f7 7b 0f

platform caam_sm: [0040] a9 11 c5 2a 09 1b b1 76

platform caam_sm: [0048] 9c 2f 93 fb f0 d2 b4 d4

platform caam_sm: [0056] c4 74 93 24 40 ef 9f 10

platform caam_sm: [0064] 26 a1 30 03 e0 bf 4a a7

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 256-bit black key in blob:

platform caam_sm: [0000] c7 80 eb a2 c8 fa 77 69

platform caam_sm: [0008] 5e 71 2f 12 9f 10 84 7f

platform caam_sm: [0016] f9 3b 4c 49 dc b0 67 b0

platform caam_sm: [0024] 87 29 60 f8 c6 6a 31 cd

platform caam_sm: [0032] 33 13 02 85 c5 19 07 17

platform caam_sm: [0040] 28 5e 00 55 5e 4e dd 17

platform caam_sm: [0048] f2 c4 a5 4a 8a e0 16 d9

platform caam_sm: [0056] d7 96 75 00 de 1e a0 d6

platform caam_sm: [0064] e4 e9 1e 44 cf c9 51 02

platform caam_sm: [0072] 48 55 c0 b4 64 d4 c4 50

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: restored 64-bit black key:

platform caam_sm: [0000] a5 68 09 f1 f4 9b 9d cf

platform caam_sm: [0008] 2b 43 45 09 ed 2f cd 92

platform caam_sm: restored 128-bit black key:

platform caam_sm: [0000] d8 3f 70 49 83 1f 78 92

platform caam_sm: [0008] b5 45 fe f4 a2 96 15 5d

platform caam_sm: restored 192-bit black key:

platform caam_sm: [0000] c1 4a 58 87 91 b7 ce a2

platform caam_sm: [0008] 36 75 ba 23 76 92 a9 46

platform caam_sm: [0016] e5 92 85 ff 10 3d d0 a0

platform caam_sm: [0024] 27 9e b0 f4 68 16 44 b7

platform caam_sm: restored 256-bit black key:

platform caam_sm: [0000] 61 c9 9e d4 9c 03 64 79

platform caam_sm: [0008] 80 4a bf 01 d8 4a 8c 5d

platform caam_sm: [0016] 27 96 b1 88 6b c5 fa e6

platform caam_sm: [0024] 18 b0 26 96 a4 6e 02 28

snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

wm8962 0-001a: Failed to read ID register

wm8962: probe of 0-001a failed with error -5

fsl-asrc 2034000.asrc: driver registered

imx-wm8962 sound.22: failed to find codec platform device

imx-wm8962: probe of sound.22 failed with error -22

imx-audio-hdmi sound-hdmi.23: hdmi-hifi <-> hdmi_audio.3 mapping ok

NET: Registered protocol family 26

TCP: cubic registered

NET: Registered protocol family 10

sit: IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

can: controller area network core (rev 20120528 abi 9)

NET: Registered protocol family 29

can: raw protocol (rev 20120528)

can: broadcast manager protocol (rev 20120528 t)

can: netlink gateway (rev 20130117) max_hops=1

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: BNEP socket layer initialized

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

Bluetooth: HIDP socket layer initialized

8021q: 802.1Q VLAN Support v1.8

Key type dns_resolver registered

VGEN3: disabling

VGEN2: disabling

VGEN1: disabling

SWBST: disabling

SW4: disabling

wm8962-supply: disabling

regulator-dummy: disabling

imx mcc test is registered.

input: gpio-keys.21 as /devices/soc0/gpio-keys.21/input/input3

snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:02 UTC (2)

ALSA device list:

  #0: imx-hdmi-soc

kjournald starting.  Commit interval 5 seconds

EXT3-fs (mmcblk2p2): using internal journal

EXT3-fs (mmcblk2p2): recovery complete

EXT3-fs (mmcblk2p2): mounted filesystem with ordered data mode

VFS: Mounted root (ext3 filesystem) on device 179:2.

devtmpfs: mounted

Freeing unused kernel memory: 336K (80d58000 - 80dac000)

INIT: version 2.88 booting

Starting udev

udev: Not using udev cache because of changes detected in the following files:

udev:     /proc/version /proc/cmdline /proc/devices

udev:     lib/udev/rules.d/* etc/udev/rules.d/*

udev: The udev cache will be regenerated. To identify the detected changes,

udev: compare the cached sysconf at   /etc/udev/cache.data

udev: against the current sysconf at  /dev/shm/udev.cache

udevd[204]: starting version 182

random: nonblocking pool is initialized

bootlogd: cannot allocate pseudo tty: No such file or directory

Populating dev cache

ALSA: Restoring mixer settings...

No state is present for card imxhdmisoc

Found hardware: "imx-hdmi-soc" "" "" "" ""

Hardware is initialized using a generic method

No state is present for card imxhdmisoc

Sun Apr 19 23:58:46 UTC 2015

INIT: Entering runlevel: 5

Configuring network interfaces... fec 2188000.ethernet eth0: no PHY, assuming direct connection to switch

libphy: PHY fixed-0:00 not found

fec 2188000.ethernet eth0: could not attach to PHY

ifconfig: SIOCSIFFLAGS: No such device

Starting system message bus: dbus.

Starting OpenBSD Secure Shell server: sshd

done.

Starting syslogd/klogd: done

Running local boot scripts (/etc/rc.local).

Poky (Yocto Project Reference Distro) 1.8 imx6qsabresd /dev/ttymxc0

imx6qsabresd login

Labels (1)
Tags (2)
1 Solution
3,597 Views
Sasamy
Contributor IV
2 Replies
3,598 Views
Sasamy
Contributor IV
3,597 Views
kikimorisato
Contributor II

Thank you for ur correct answer!!!

0 Kudos
Reply