Yocto Kernel 3.10.17 bad CRC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto Kernel 3.10.17 bad CRC

Jump to solution
1,894 Views
vasileiostzizil
Contributor III

Hello all

I am trying to load the yocto with the kernel 3.10.17 through the sdcard.

I followed the instructions and through the dd command I wrote the image to the card.

The sambresd imx6 starts but after some seconds I am getting the message Kernel ... bad CRC and then it gets me to the Uboot console.

If there any isssue with that kernel?

Thank you

Vasilis

Labels (1)
0 Kudos
Reply
1 Solution
1,728 Views
OtavioSalvador
Senior Contributor II

Usually this type of error is a bad uSD card or card adapter.

View solution in original post

0 Kudos
Reply
3 Replies
1,728 Views
yanfengliu
Contributor III

Probably you need check the u-boot parameters, the ones listed in the section 8.2 of the user guide document is somehow wrong. I can boot the device by making the following changes:

  • "root=/dev/mmcblk0p2"  should be "root=/dev/mmcblk0p1" in my case since the guide only created one partition on the SD card;
  • "mmc read ${loadaddr} 0x800 0x2000" should be "mmc read ${loadaddr} 0x800 0x4000" actually since 0x800000bytes means 0x4000 blocks if each block has 0x200 (512) bytes

Please try it and let me know if this helps.

0 Kudos
Reply
1,728 Views
OtavioSalvador
Senior Contributor II

vasileiostzizilonis problem has been solved already. It was the uSD card or card adapter.         

0 Kudos
Reply
1,729 Views
OtavioSalvador
Senior Contributor II

Usually this type of error is a bad uSD card or card adapter.

0 Kudos
Reply