Yocto Installation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Yocto Installation

1,483 次查看
1990rahulreddy
Contributor IV

ERROR: Task 672 (/home/rahul/fsl-release-bsp/sources/poky/meta/recipes-devtools/gcc/gcc-cross-initial_4.9.bb, do_compile) failed with exit code '1'

what packages are missing, I have foolow pdf, YOcto start guide...

标签 (2)
0 项奖励
回复
1 回复

1,259 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please try the recent NXP BSP. Follow exactly recommendations of "

Freescale Yocto Project User's Guide" in docs.

http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS&Parent_nodeId=13376994810717061...

Summary page :

i.MX 6 Series Software and Development Tool|NXP

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复