[Yocto] How to install file to rootfs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Yocto] How to install file to rootfs

Jump to solution
7,780 Views
WolsYang
Contributor IV

Hi NXP,

I am trying to install the file to rootfs but fail.

Here is my env

BB_VERSION           = "2.0.0"
BUILD_SYS            = "x86_64-linux"
NATIVELSBSTRING      = "universal"
TARGET_SYS           = "aarch64-poky-linux"
MACHINE              = "imx8qxpc0mek"
DISTRO               = "fsl-imx-wayland"
DISTRO_VERSION       = "5.15-kirkstone"
TUNE_FEATURES        = "aarch64 armv8a crc crypto"

Here is my recipe "test.bb"

DESCRIPTION = "Box software"
LICENSE = "CLOSED"
# FILESEXTRAPATHS:prepend := "${THISDIR}/${PN}:"
SRC_URI += " \
    file://test \
    "
S = "${WORKDIR}"

do_install:append() {
    bbwarn "Test install file to rootfs <<<<<<<<<<<<<<<"
    #WiFi	
    install -D -v -m 0755 test -t ${D}${ROOT_HOME}/
}
FILES:${PN} += "${ROOT_HOME}/*"

 And here is the error output

ERROR: imx-image-multimedia-1.0-r0 do_rootfs: Unable to install packages. Command '/media/wols/Data-ext4/imx5.15.52/clean_build/tmp/work/imx8qxpc0mek-poky-linux/imx-image-multimedia/1.0-r0/recipe-sysroot-native/usr/bin/apt-get  install --allow-downgrades --allow-remove-essential --allow-change-held-packages --allow-unauthenticated --no-remove apt docker dpkg firmwared imx-g2d-samples packagegroup-base-extended packagegroup-core-boot packagegroup-core-full-cmdline packagegroup-core-nfs-server packagegroup-core-sdk packagegroup-core-ssh-dropbear packagegroup-core-standalone-sdk-target packagegroup-core-tools-debug packagegroup-core-tools-profile packagegroup-core-tools-testapps packagegroup-core-weston packagegroup-fsl-gstreamer1.0 packagegroup-fsl-gstreamer1.0-full packagegroup-fsl-optee-imx packagegroup-fsl-tools-audio packagegroup-fsl-tools-benchmark packagegroup-fsl-tools-gpu packagegroup-fsl-tools-gpu-external packagegroup-fsl-tools-testapps packagegroup-imx-isp packagegroup-imx-security packagegroup-tools-bluetooth run-postinsts test' returned 100:

Reading package lists...
Building dependency tree...
Reading state information...

Some packages could not be installed. This may mean that you have
requested an impossible situation or if you are using the unstable
distribution that some required packages have not yet been created
or been moved out of Incoming.
The following information may help to resolve the situation:

The following packages have unmet dependencies:
 packagegroup-fsl-tools-testapps : Depends: cryptodev-module but it is not installable
E: Unable to correct problems, you have held broken packages.

I also try add < IMAGE_INSTALL:append = " cryptodev-module " >

But it dosen help , another error came out.

The following packages have unmet dependencies:
 kernel-module-cryptodev-5.15.52+g8e9642731c85 : Depends: kernel-5.15.52+g8e9642731c85 but it is not installable
0 Kudos
Reply
1 Solution
7,758 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @WolsYang,

I hope you are doing well.

Please make sure that there is not any other recipe named test.

Please uncomment FILESEXTRAPATHS:prepend in receipe. (this specifies the path where the binary file is present)

Please make sure that the test binary is placed at <..>/test directory.

Please provide me with directory structure of recipe for further debugging. (using tree command)

Thanks & Regards,
Dhruvit Vasavada

View solution in original post

0 Kudos
Reply
4 Replies
7,759 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @WolsYang,

I hope you are doing well.

Please make sure that there is not any other recipe named test.

Please uncomment FILESEXTRAPATHS:prepend in receipe. (this specifies the path where the binary file is present)

Please make sure that the test binary is placed at <..>/test directory.

Please provide me with directory structure of recipe for further debugging. (using tree command)

Thanks & Regards,
Dhruvit Vasavada

0 Kudos
Reply
7,707 Views
WolsYang
Contributor IV

Hi @Dhruvit ,

    Sorry for the late reply.

    Since I delete tmp & sstate then rebuild, this issue gone.

    I think is state problem.

meta-test
├── conf
│   └── layer.conf
├── recipes-driver
│   └── test
│       ├── test
│       │   └── test
│       └── test.bb


 

0 Kudos
Reply
7,702 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @WolsYang,

I hope you are doing well.

Glad to know that issue is resolved.

Can I mark this case as close now?

Thanks & Regards,
Dhruvit Vasavada

 

0 Kudos
Reply
7,697 Views
WolsYang
Contributor IV

Hi @Dhruvit 

        Sure : )

0 Kudos
Reply