Yocto GStreamer Video Problem [fsl-image-fb]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto GStreamer Video Problem [fsl-image-fb]

13,464 Views
sumanranjan
Contributor III

Board : imx6sabresd quadcore board

Recipe : fsl-image-fb

Step 1: get the code

$ mkdir fsl-community-bsp

$ cd fsl-community-bsp

$ repo init -u http://github.com/Freescale/fsl-community-bsp-platform -b dora

$ mv .repo/manifest.xml .repo/manifest.orig #remove community manifest

$  cp <location>/fsl-yocto-release-manifest.xml .repo/manifest.xml #replace with freescale manifest.xml within Yocto Release

$ repo sync #sync the repo

$ cp -r sources/meta-fsl-bsp-release/imx/meta-fsl-arm/conf/machine sources/metafsl-arm/conf # This step copies the new machine configuration files into the meta-fsl-arm so that

# community setup can find new machine files.

Step 2: build it

$ MACHINE=imx6qsabresd source setup-environment build-fb

$ cd ..

$ source fsl-setup-release.sh -b build-fb -e fb

$ bitbake fsl-image-fb


Things build OK and graphics OpenGL/ES tests run fine on imx6sabresd board. However, GStreamer has a problem in this image. First of all, I see that only few GStreamer plugins are copied to filesystem rootfs, but many plugins are present in 'sysroot' folder. Why this is so ??


1. gst-inspect command shows very few plugins.

Total count: 4 plugins, 26 features

   When I checked in the "sysroot" of the build folder I found many plugins were present : ../fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/lib/gstreamer-0.10. I copied all plugins from sysroot folder  

   to rootfs folder ( /usr/lib/).

    After this gst-inspect shows many plugins.

Total count: 177 plugins (1 blacklist entry not shown), 594 features


After copying plugins from sysroot folder below tests pass.


a. .264 file is playing successfully.

gst-launch filesrc location=FVDO_Plane_4cif.264 typefind=true ! vpudec ! mfw_v4lsink


b. rtsp camera stream is decoded successfully.

gst-launch rtspsrc location=rtsp://10.20.1.48/axis-media/media.amp typefind=true !  gstrtpjitterbuffer ! rtph264depay queue-delay=0 ! capsfilter caps="video/x-h264,width=640,height=480,framerate=(fraction)30/1" ! vpudec low-latency=true ! queue max-size-buffers=0 max-size-time=0 ! mfw_v4lsink sync=false



2. Before copying plugins from sysroot 'aiurdemux' was not even present, but after copy 'aiurdemux' shows up in 'gst-inspect' command and throws following error.


# gst-inspect aiurdemux

  

(gst-inspect-0.10:666): GStreamer-CRITICAL **: gst_element_class_add_pad_template: assertion `GST_IS_PAD_TEMPLATE (templ)' failed

(gst-inspect-0.10:666): GStreamer-CRITICAL **: gst_pad_new_from_template: assertion `GST_IS_PAD_TEMPLATE (templ)' failed

(gst-inspect-0.10:666): GStreamer-CRITICAL **: gst_pad_set_activate_function: assertion `GST_IS_PAD (pad)' failed

(gst-inspect-0.10:666): GStreamer-CRITICAL **: gst_pad_set_activatepull_function: assertion `GST_IS_PAD (pad)' failed

(gst-inspect-0.10:666): GStreamer-CRITICAL **: gst_pad_set_activatepush_function: assertion `GST_IS_PAD (pad)' failed

(gst-inspect-0.10:666): GStreamer-CRITICAL **: gst_pad_set_chain_function: assertion `GST_IS_PAD (pad)' failed

(gst-inspect-0.10:666): GStreamer-CRITICAL **: gst_pad_set_event_function: assertion `GST_IS_PAD (pad)' failed

(gst-inspect-0.10:666): GStreamer-CRITICAL **: gst_element_add_pad: assertion `GST_IS_PAD (pad)' failed

(gst-inspect-0.10:666): GStreamer-CRITICAL **: gst_pad_set_setcaps_function: assertion `GST_IS_PAD (pad)' failed

Factory Details:

  Long name:    aiur universal demuxer

  Class:        Codec/Demuxer

  Description:  demux container file to video, audio, and subtitle

  Author(s):    Multimedia Team <[email protected]>

  Rank:         primary + 1 (257)

Plugin Details:

  Name:                 aiur.imx

  Description:          aiur universal demux/mux

  Filename:             /usr/lib/gstreamer-0.10/libmfw_gst_aiur_demux.so

  Version:              3.0.9

  License:              LGPL

  Source module:        gst-fsl-plugins

  Binary package:       Freescle Gstreamer Multimedia Plugins

  Origin URL:           http://www.freescale.com


3. MP4 video fails to play using GStreamer pipeline.

    gst-launch filesrc location=test.mp4 typefind=true ! aiurdemux ! vpudec ! mfw_v4lsink  

Logs:

(gst-launch-0.10:684): GStreamer-CRITICAL **: gst_element_class_add_pad_template: assertion `GST_IS_PAD_TEMPLATE (templ)' failed

(gst-launch-0.10:684): GStreamer-CRITICAL **: gst_pad_new_from_template: assertion `GST_IS_PAD_TEMPLATE (templ)' failed

(gst-launch-0.10:684): GStreamer-CRITICAL **: gst_pad_set_activate_function: assertion `GST_IS_PAD (pad)' failed

(gst-launch-0.10:684): GStreamer-CRITICAL **: gst_pad_set_activatepull_function: assertion `GST_IS_PAD (pad)' failed

(gst-launch-0.10:684): GStreamer-CRITICAL **: gst_pad_set_activatepush_function: assertion `GST_IS_PAD (pad)' failed

(gst-launch-0.10:684): GStreamer-CRITICAL **: gst_pad_set_chain_function: assertion `GST_IS_PAD (pad)' failed

(gst-launch-0.10:684): GStreamer-CRITICAL **: gst_pad_set_event_function: assertion `GST_IS_PAD (pad)' failed

(gst-launch-0.10:684): GStreamer-CRITICAL **: gst_element_add_pad: assertion `GST_IS_PAD (pad)' failed

(gst-launch-0.10:684): GStreamer-CRITICAL **: gst_pad_set_setcaps_function: assertion `GST_IS_PAD (pad)' failed

MFW_GST_V4LSINK_PLUGIN 3.0.9 build on Apr 11 2014 10:15:40.

WARNING: erroneous pipeline: could not link filesrc0 to aiurdemux0

4. I have another yocto setup with 'fsl-image-gui'. Running the same MP4 playback pipeline works fine. The difference I can make out is in the library version of 'aiurdemux' . 'fsl-image-gui' is using 3.0.5 and 'fsl-image-fb' is using 3.0.9 of 'aiurdemux'.

root@imx6qsabresd:/usr/lib/gstreamer-0.10# gst-inspect aiurdemux

Factory Details:

  Long name:    aiur universal demuxer

  Class:        Codec/Demuxer

  Description:  demux container file to video, audio, and subtitle

  Author(s):    Multimedia Team <[email protected]>

  Rank:         primary + 1 (257)

Plugin Details:

  Name:                 aiur.imx

  Description:          aiur universal demux/mux

  Filename:             /usr/lib/gstreamer-0.10/libmfw_gst_aiur_demux.so

  Version:              3.0.5

  License:              LGPL

  Source module:        gst-fsl-plugins

  Binary package:       Freescle Gstreamer Multimedia Plugins

  Origin URL:           http://www.freescale.com.

Questions:

1. Why most of the compiled plugins are present in 'sysroot' folder instead of '/usr/lib' folder ? Do you think that copying those plugins from 'sysroot' to rootfs may create any issue ? 'aiurdemux' is one thing that I see creating issue right now(after sysroot copy) and other pipelines e.g. RTSP and .264 file decoding works without any problem.

2. Has anyone tested 3.0.9 version of 'aiurdemux' on sabresd board with 'fsl-image-fb' recipe ?

3. How should I fix this issue ?

Labels (1)
19 Replies

8,155 Views
daiane_angolini
NXP Employee
NXP Employee

1. Why most of the compiled plugins are present in 'sysroot' folder instead of '/usr/lib' folder ? Do you think that copying those plugins from 'sysroot' to rootfs may create any issue ? 'aiurdemux' is one thing that I see creating issue right now(after sysroot copy) and other pipelines e.g. RTSP and .264 file decoding works without any problem.


One thing is to build, another is to "install". The folder sysroot is used by BitBake to store a copy of sysroot *during* the build. It's a temp dir and there is no warranty is it's going to be good or not. I mean, the complete directory, all binaries are OK.

2. Has anyone tested 3.0.9 version of 'aiurdemux' on sabresd board with 'fsl-image-fb' recipe ?


Yes I have. In fact I just realized several tests (however with only 3 different files/codecs) using gplay (that uses aiurdemux by default) and it worked perfectly on imx6qsabresd board, however I tested using the FSL Community BSP image called fsl-image-machine-test, for all 3 backends (X11, DFB, WL, X11). And I used master. It was part of my test for next YP release 1.7 And the MM version on master today is 3.0.10.



https://github.com/Freescale/meta-fsl-demos/blob/master/recipes-fsl/packagegroups/packagegroup-fsl-g...


It's not available on your source code (you're using dora, and the file I sent you is only available on master) but in this file you understand how you can add ALL gstreamer plugins available

3. How should I fix this issue ?


Take a loon in this file:


https://github.com/Freescale/meta-fsl-demos/blob/master/recipes-fsl/packagegroups/packagegroup-fsl-g...


Please, report your progress.

0 Kudos
Reply

8,155 Views
sumanranjan
Contributor III

Thanks Daiane.

2. Has anyone tested 3.0.9 version of 'aiurdemux' on sabresd board with 'fsl-image-fb' recipe ?


Yes I have. In fact I just realized several tests (however with only 3 different files/codecs) using gplay (that uses aiurdemux by default) and it worked perfectly on imx6qsabresd board, however I tested using the FSL Community BSP image called fsl-image-machine-test, for all 3 backends (X11, DFB, WL, X11). And I used master. It was part of my test for next YP release 1.7 And the MM version on master today is 3.0.10.


I am able to play MP4 video file using 'gplay' which should be using 'aiurdemux' by default. However, as I have mentioned in my post above that using the pipeline it does not work.

Have you tested by running the pipeline instead of 'gplay' ? Do you see anything wrong with my pipeline command ?


I will download and test the image you have shared and let you know the results.



Regarding GStreamer plugin present in sysroot instead of rootfs folder. Below is what I did in order to make GStreamer a part of filesystem.

  • Edit fsl-image-fb.bb
  • Add ‘packagegroup-fsl-gstreamer’ into IMAGE_INSTALL option.

$ vi fsl-community-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-demos/recipes-fsl/images/fsl-image-fb.bb

…..

IMAGE_INSTALL += " \

${SOC_IMAGE_INSTALL} \

cpufrequtils \

nano \

    packagegroup-fsl-gstreamer \

packagegroup-fsl-tools-testapps \

packagegroup-fsl-tools-benchmark \

    "

……


8,155 Views
sumanranjan
Contributor III

I tested with the filesystem you gave in the link : fsl-image-machine-test-imx6qsabresd-20140421-122.rootfs.tar.bz2

Observation:

1. 'gplay' works fine as usual.

2. GStreamer pipeline fails to decode with following error,

root@imx6qsabresd:/unit_tests# gst-launch filesrc location=akiyo.mp4 typefind=true ! aiurdemux ! vpudec ! mfw_v4lsink

MFW_GST_V4LSINK_PLUGIN 3.0.10 build on Apr 19 2014 22:19:35.

Setting pipeline to PAUSED ...

[INFO]  Product Info: i.MX6Q/D/S

vpudec versions :smileyhappy:

        plugin: 3.0.10

        wrapper: 1.0.45(VPUWRAPPER_ARM_LINUX Build on Apr 19 2014 22:17:04)

        vpulib: 5.4.20

        firmware: 2.3.10.40778

Pipeline is PREROLLING ...

(gst-launch-0.10:1246): GStreamer-CRITICAL **: gst_mini_object_unref: assertion 'GST_IS_MINI_OBJECT (mini_object)' failed

(gst-launch-0.10:1246): GStreamer-CRITICAL **: gst_mini_object_unref: assertion 'GST_IS_MINI_OBJECT (mini_object)' failed

(gst-launch-0.10:1246): GStreamer-CRITICAL **: gst_mini_object_unref: assertion 'GST_IS_MINI_OBJECT (mini_object)' failed

(gst-launch-0.10:1246): GStreamer-CRITICAL **: gst_mini_object_unref: assertion 'GST_IS_MINI_OBJECT (mini_object)' failed

(gst-launch-0.10:1246): GStreamer-CRITICAL **: gst_mini_object_unref: assertion 'GST_IS_MINI_OBJECT (mini_object)' failed

(gst-launch-0.10:1246): GStreamer-CRITICAL **: gst_mini_object_unref: assertion 'GST_IS_MINI_OBJECT (mini_object)' failed

....

It continue to throw this error until the playback is over. No Video output on the screen.

Please provide your inputs.

0 Kudos
Reply

8,155 Views
daiane_angolini
NXP Employee
NXP Employee

So, when you included all gstreamer packages on the previous release, you was able to get gplay working?

Have you double checked the codec used in the file akiyo.mp4 ?

This file used to be a "pure mp4" file with no "container", when I used this file it was with no demuxer in the gst command line

Could you, please, double check?

I'm sorry for not seeing that before

0 Kudos
Reply

8,155 Views
sumanranjan
Contributor III

I am not sure what you mean by "pure mp4" file. MP4 itself is a container to host video & audio (h264+aac).  I guess you mean "akiyo.mp4" has only h264 video component and no audio component. Even that being the case, we would require 'aiurdemux' to fetch h264 video out from MP4 container. I tried with many MP4 files with video+audio but all result in the same error as above.

0 Kudos
Reply

8,155 Views
LeonardoSandova
Specialist I

Suman, please enable logging with --gst-debug=*:2,GST_ELEMENT_FACTORY:3 as extra parameter on either gplay and gst-launch. This will allow us to see any error and the elements being instantiated.

8,155 Views
sumanranjan
Contributor III

I was on vacation so couldn't reply earlier. I run the test on build-fb image and got the below error log.

$ gst-launch --gst-debug=*:2,GST_ELEMENT_FACTORY:3 filesrc location=akiyo.mp4 typefind=true ! aiurdemux ! vpudec ! mfw_v4lsink

0:00:00.084199667   718  0x1145880 INFO     GST_ELEMENT_FACTORY /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstelementfactory.c:376:gst_element_factory_create: creating element "filesrc"

0:00:00.090680667   718  0x1145880 INFO     GST_ELEMENT_FACTORY /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstelementfactory.c:376:gst_element_factory_create: creating element "aiurdemux"

(gst-launch-0.10:718): GStreamer-CRITICAL **: gst_debug_log_valist: assertion `category != NULL' failed

0:00:00.095228667   718  0x1145880 INFO     GST_ELEMENT_FACTORY /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstelementfactory.c:376:gst_element_factory_create: creating element "vpudec"

0:00:00.101644667   718  0x1145880 INFO     GST_ELEMENT_FACTORY /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstelementfactory.c:376:gst_element_factory_create: creating element "mfw_v4lsink"

0:00:00.112594667   718  0x1145880 WARN             mfw_v4lsink mfw_gst_v4lsink.c:303:mfw_gst_v4l2sink_query_support_formats: unrecognized format:[Y444]YUV444

MFW_GST_V4LSINK_PLUGIN 3.0.9 build on Apr 24 2014 17:25:24.

0:00:00.114548667   718  0x1145880 INFO     GST_ELEMENT_FACTORY /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstelementfactory.c:376:gst_element_factory_create: creating element "pipeline"

Setting pipeline to PAUSED ...

[INFO]  Product Info: i.MX6Q/D/S

vpudec versions :smileyhappy:

        plugin: 3.0.9

        wrapper: 1.0.40(VPUWRAPPER_ARM_LINUX Build on Apr 24 2014 16:53:25)

        vpulib: 5.4.18

        firmware: 2.3.10.40778

Pipeline is PREROLLING ...

0:00:00.163790000   718  0x117b4f0 WARN          GST_SCHEDULING /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstpad.c:5183:gst_pad_pull_range:<aiurdemux0:sink> pullrange returned buffer of different caps

(gst-launch-0.10:718): GStreamer-CRITICAL **: gst_mini_object_unref: assertion `GST_IS_MINI_OBJECT (mini_object)' failed

0:00:00.164088667   718  0x117b4f0 WARN          GST_SCHEDULING /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstpad.c:5183:gst_pad_pull_range:<aiurdemux0:sink> pullrange returned buffer of different caps

(gst-launch-0.10:718): GStreamer-CRITICAL **: gst_mini_object_unref: assertion `GST_IS_MINI_OBJECT (mini_object)' failed

0:00:00.164300000   718  0x117b4f0 WARN          GST_SCHEDULING /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstpad.c:5183:gst_pad_pull_range:<aiurdemux0:sink> pullrange returned buffer of different caps

(gst-launch-0.10:718): GStreamer-CRITICAL **: gst_mini_object_unref: assertion `GST_IS_MINI_OBJECT (mini_object)' failed

0:00:00.164503333   718  0x117b4f0 WARN          GST_SCHEDULING /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstpad.c:5183:gst_pad_pull_range:<aiurdemux0:sink> pullrange returned buffer of different caps

(gst-launch-0.10:718): GStreamer-CRITICAL **: gst_mini_object_unref: assertion `GST_IS_MINI_OBJECT (mini_object)' failed

0:00:00.164703333   718  0x117b4f0 WARN          GST_SCHEDULING /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstpad.c:5183:gst_pad_pull_range:<aiurdemux0:sink> pullrange returned buffer of different caps

(gst-launch-0.10:718): GStreamer-CRITICAL **: gst_mini_object_unref: assertion `GST_IS_MINI_OBJECT (mini_object)' failed

0:00:00.164904667   718  0x117b4f0 WARN          GST_SCHEDULING /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstpad.c:5183:gst_pad_pull_range:<aiurdemux0:sink> pullrange returned buffer of different caps

(gst-launch-0.10:718): GStreamer-CRITICAL **: gst_mini_object_unref: assertion `GST_IS_MINI_OBJECT (mini_object)' failed

0:00:00.165095333   718  0x117b4f0 WARN          GST_SCHEDULING /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstpad.c:5183:gst_pad_pull_range:<aiurdemux0:sink> pullrange returned buffer of different caps

(gst-launch-0.10:718): GStreamer-CRITICAL **: gst_mini_object_unref: assertion `GST_IS_MINI_OBJECT (mini_object)' failed

0:00:00.496650333   718  0x117b4f0 WARN          GST_SCHEDULING /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstpad.c:5183:gst_pad_pull_range:<aiurdemux0:sink> pullrange returned buffer of different caps

(gst-launch-0.10:718): GStreamer-CRITICAL **: gst_mini_object_unref: assertion `GST_IS_MINI_OBJECT (mini_object)' failed

0:00:00.497045000   718  0x117b4f0 WARN          GST_SCHEDULING /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstpad.c:5183:gst_pad_pull_range:<aiurdemux0:sink> pullrange returned buffer of different caps

(gst-launch-0.10:718): GStreamer-CRITICAL **: gst_mini_object_unref: assertion `GST_IS_MINI_OBJECT (mini_object)' failed

0:00:00.497415000   718  0x117b4f0 WARN          GST_SCHEDULING /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstpad.c:5183:gst_pad_pull_range:<aiurdemux0:sink> pullrange returned buffer of different caps

(gst-launch-0.10:718): GStreamer-CRITICAL **: gst_mini_object_unref: assertion `GST_IS_MINI_OBJECT (mini_object)' failed

0:00:00.497786667   718  0x117b4f0 WARN          GST_SCHEDULING /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstpad.c:5183:gst_pad_pull_range:<aiurdemux0:sink> pullrange returned buffer of different caps

0 Kudos
Reply

8,155 Views
LeonardoSandova
Specialist I

Suman, can you run gplay with --gst-debug params? Post results. There must be some missing element manual pipeline.

0 Kudos
Reply

8,155 Views
sumanranjan
Contributor III

Debug Logs does not with GPLAY Utility:

---------------------------------------------------------------

#gst-launch --gst-debug=*:2,GST_ELEMENT_FACTORY:3 gplay The_Sorcere_480p.mp4

0:00:00.069581000   722   0x9fd880 INFO     GST_ELEMENT_FACTORY /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/gstelementfactory.c:467:gst_element_factory_make: no such element factory "gplay"!

0:00:00.069790000   722   0x9fd880 ERROR           GST_PIPELINE /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/parse/grammar.y:661:priv_gst_parse_yyparse: no element "gplay"

0:00:00.069877667   722   0x9fd880 ERROR           GST_PIPELINE /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/parse/grammar.y:929:priv_gst_parse_launch: Unrecoverable syntax error while parsing pipeline gplay The_Sorcere_480p.mp4

ERROR: pipeline could not be constructed: no element "gplay".

#gst-launch --gst-debug=*:2 gplay The_Sorcere_480p.mp4

0:00:00.067488000   706  0x1072880 ERROR           GST_PIPELINE /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/parse/grammar.y:661:priv_gst_parse_yyparse: no element "gplay"

0:00:00.067701333   706  0x1072880 ERROR           GST_PIPELINE /home/suman/fsl-community-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/gst/parse/grammar.y:929:priv_gst_parse_launch: Unrecoverable syntax error while parsing pipeline gplay The_Sorcere_480p.mp4

ERROR: pipeline could not be constructed: no element "gplay".

Is there some other way to add debug logs with 'gplay' ?

0 Kudos
Reply

8,155 Views
YixingKong
Senior Contributor IV

Suman

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos
Reply

8,155 Views
YixingKong
Senior Contributor IV

Suman

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

8,155 Views
daiane_angolini
NXP Employee
NXP Employee

$ export GST_DEBUG=3

$ gplay abc.mp4

0 Kudos
Reply

8,155 Views
daiane_angolini
NXP Employee
NXP Employee

This is the working command line:

gst-launch filesrc location= akiyo.mp4 ! 'video/mpeg, systemstream=(boolean)false , mpegversion=(int)4' ! vpudec ! mfw_v4lsink

The file is a raw file, with no container needed, the only needed additional parameters is the explicit cap to inform vpudec how to proceed.

I hope this can help ;-)

8,156 Views
sumanranjan
Contributor III

The command provided by you works fine for akiyo.mp4 file.:smileyhappy:

How about general MP4 ( H264 + AAC ) where 'aiurdemux' is required ? Can you please provide pipeline to run the MP4 files.

0 Kudos
Reply

8,156 Views
LeonardoSandova
Specialist I

Suman,

auiurdemux is a demuxer, so it is used on containers. I wonder if the command 'file' would give some insight of the media file type...

The easiest way to do a playback is through gplay or 'gst-launch playbin2' unless you have a reason to play it manually..

Leo

0 Kudos
Reply

8,156 Views
daiane_angolini
NXP Employee
NXP Employee

I tested and saw exactly the same error.

Gplay works

decodebin works

playbin works

the explicit command line does not work.

I'm working to understand what's the missing part of the pipeline. When I have an update I let you know

0 Kudos
Reply

8,156 Views
daiane_angolini
NXP Employee
NXP Employee

:smileygrin: yes, everything that you said is right :smileygrin:

I must keep a lot of things in my mind, and sometimes (usually) I mix them up. Usually when talking about version number... Sorry.

I would need to reproduce it by myself, but I would only be able to test it on next Monday. If you could not wait I will need to ask for re-assign. Please, let me know.

0 Kudos
Reply

8,156 Views
daiane_angolini
NXP Employee
NXP Employee

oh, I forgot to say one thing.

You can, for sure, trick the installation system and copy one binary over the sysroot dir to your sdcard. It's not beaustifull, it's not clean, but it works! It works but in case the binary depends on another binary files. And in case of aiurdemux that's the case! It depends on several other .so files, in a tied directory tree.

0 Kudos
Reply

8,156 Views
daiane_angolini
NXP Employee
NXP Employee

if you want to take a look in the image I tested you can see it here:

The direct link is the following, but it should not work forever:

http://ci.ossystems.com.br/public/fsl-community-bsp/master/122

For the permanent link, see FSL Community BSP

0 Kudos
Reply