Yocto Error : do_compile error while adding meta-webkit layer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto Error : do_compile error while adding meta-webkit layer

ソリューションへジャンプ
10,962件の閲覧回数
Muthyam
Contributor I

Hello community, i am working on VAR-SOM IMX8 and i am building a Qt5 image, the yocto version is dunfell-fslc-5.4-2.1.x-mx8-v1.5. When i tried to meta-webkit layer to it i a getting error

ERROR: Task (/home/medha/var-fslc-yocto/sources/meta-webkit/recipes-browser/wpewebkit/wpewebkit_2.32.1.bb:do_compile) failed with exit code '1'

The process that i followed is

1.Add meta-webkit layer
    git clone https://github.com/Igalia/meta-webkit -b dunfell
2. Make sure to add layer to conf/bblayers.conf
3.Add additional packages to the build via local.conf
    IMAGE_INSTALL_append = " wpewebkit cog"

    PREFERRED_PROVIDER_virtual/wpebackend = "wpebackend-fdo"

4.Build the image -> bitbake fsl-image-qt5
 
 

medha@C2680:~/var-fslc-yocto/build_xwayland$ bitbake fsl-image-qt5


WARNING: You have included the meta-virtualization layer, but 'virtualization' has not been enabled in your DISTRO_FEATURES. Some bbappend files may not take effect. See the meta-virtualization README for details on enabling virtualization support.
Loading cache: 100% |##########################################################################################################################| Time: 0:00:00
Loaded 3903 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.46.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "aarch64-fslc-linux"
MACHINE = "imx8qm-var-som"
DISTRO = "fslc-xwayland"
DISTRO_VERSION = "3.1"
TUNE_FEATURES = "aarch64 armv8a crc crypto cortexa72-cortexa53"
TARGET_FPU = ""
meta
meta-poky = "HEAD:2a848e95074318f3a243df7b3f40513a13173a82"
meta-oe
meta-multimedia
meta-python
meta-filesystems
meta-gnome
meta-networking = "HEAD:7bd47ef6c98323c95a9e527129dca98c9a65ee08"
meta-freescale = "HEAD:12c3eed6a90b436565126d8ba6934f794b816e25"
meta-freescale-3rdparty = "HEAD:537cb85e4db17d1f6b356a92112b32ae2e39b235"
meta-freescale-distro = "HEAD:5d882cdf079b3bde0bd9869ce3ca3db411acbf3b"
meta-qt5 = "HEAD:b4d24d70aca75791902df5cd59a4f4a54aa4a125"
meta-swupdate = "HEAD:72b493c7ed9f5e1fb4ae1ce180f913acc29748c5"
meta-virtualization = "HEAD:758868633be479f38d19c3602be0094289fc1a75"
meta-variscite-fslc = "HEAD:4720596b99029cd2cb5db7bef16b41cc473a759b"
meta-variscite-hab = "HEAD:ef52ce53d860f0552dd892874cfce62537f6564a"
meta-webkit = "dunfell:270599a765743c2db5a96195b7f83877cde5d499"

WARNING: /home/medha/var-fslc-yocto/sources/meta-variscite-fslc/recipes-kernel/linux/linux-variscite_5.4.bb:do_compile is tainted from a forced runA: 0:00:01
Initialising tasks: 100% |#####################################################################################################################| Time: 0:00:03
Sstate summary: Wanted 15 Found 3 Missed 12 Current 3808 (20% match, 99% complete)
NOTE: Executing Tasks
Currently 1 running tasks (4810 of 9214) 52% |######################################################## |
0: wpewebkit-2.32.1-r0 do_compile (pid 16511) 0% |

after some time i am getting error like

......-mx8-fslc-linux/wpewebkit/2.32.1-r0/recipe-sysroot/usr/include/orc-0.4 -isystem /home/medha/var-fslc-yocto/build_xwayland/tmp/work/aarch64-mx8-fslc-linux/wpewebkit/2.32.1-r0/recipe-sysroot/usr/lib/gstreamer-1.0/include -isystem /home/medha/var-fslc-yocto/build_xwayland/tmp/work/aarch64-mx8-fslc-linux/wpewebkit/2.32.1-r0/recipe-sysroot/usr/include/libsoup-2.4 -isystem /home/medha/var-fslc-yocto/build_xwayland/tmp/work/aarch64-mx8-fslc-linux/wpewebkit/2.32.1-r0/recipe-sysroot/usr/include/gio-unix-2.0 -isystem /home/medha/var-fslc-yocto/build_xwayland/tmp/work/aarch64-mx8-fslc-linux/wpewebkit/2.32.1-r0/recipe-sysroot/usr/include/libmount -isystem /home/medha/var-fslc-yocto/build_xwayland/tmp/work/aarch64-mx8-fslc-linux/wpewebkit/2.32.1-r0/recipe-sysroot/usr/include/blkid -fdiagnostics-color=always -Wextra -Wall -Wno-expansion-to-defined -Wno-noexcept-type -Wno-psabi -Wno-misleading-indentation -Wno-maybe-uninitialized -Wwrite-strings -Wundef -Wpointer-arith -Wmissing-format-attribute -Wformat-security -Wcast-align -Wno-tautological-compare -march=armv8-a+crc+crypto -mtune=cortex-a72.cortex-a53 -fstack-protector-strong -D_FORTIFY_SOURCE=2 -Wformat -Wformat-security -Werror=format-security --sysroot=/home/medha/var-fslc-yocto/build_xwayland/tmp/work/aarch64-mx8-fslc-linux/wpewebkit/2.32.1-r0/recipe-sysroot -O2 -pipe -feliminate-unused-debug-types -fmacro-prefix-map=/home/medha/var-fslc-yocto/build_xwayland/tmp/work/aarch64-mx8-fslc-linux/wpewebkit/2.32.1-r0=/usr/src/debug/wpewebkit/2.32.1-r0 -fdebug-prefix-map=/home/medha/var-fslc-yocto/build_xwayland/tmp/work/aarch64-mx8-fslc-linux/wpewebkit/2.32.1-r0=/usr/src/debug/wpewebkit/2.32.1-r0 -fdebug-prefix-map=/home/medha/var-fslc-yocto/build_xwayland/tmp/work/aarch64-mx8-fslc-linux/wpewebkit/2.32.1-r0/recipe-sysroot= -fdebug-prefix-map=/home/medha/var-fslc-yocto/build_xwayland/tmp/work/aarch64-mx8-fslc-linux/wpewebkit/2.32.1-r0/recipe-sysroot-native= -fvisibility-inlines-hidden -march=armv8-a+crc+crypto -mtune=cortex-a72.cortex-a53 -fstack-protector-strong -D_FORTIFY_SOURCE=2 -Wformat -Wformat-security -Werror=format-security --sysroot=/home/medha/var-fslc-yocto/build_xwayland/tmp/work/aarch64-mx8-fslc-linux/wpewebkit/2.32.1-r0/recipe-sysroot -fno-strict-aliasing -fno-exceptions -fno-rtti -DNDEBUG -fPIC -DLINUX -DWL_EGL_PLATFORM -std=c++17 -MD -MT Source/WebCore/CMakeFiles/WebCore.dir/__/__/DerivedSources/WebCore/unified-sources/UnifiedSource-3a52ce78-57.cpp.o -MF Source/WebCore/CMakeFiles/WebCore.dir/__/__/DerivedSources/WebCore/unified-sources/UnifiedSource-3a52ce78-57.cpp.o.d -o Source/WebCore/CMakeFiles/WebCore.dir/__/__/DerivedSources/WebCore/unified-sources/UnifiedSource-3a52ce78-57.cpp.o -c DerivedSources/WebCore/unified-sources/UnifiedSource-3a52ce78-57.cpp
| ninja: build stopped: subcommand failed.
| WARNING: exit code 1 from a shell command.
|
ERROR: Task (/home/medha/var-fslc-yocto/sources/meta-webkit/recipes-browser/wpewebkit/wpewebkit_2.32.1.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3647 tasks of which 3638 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 2 seconds

Summary: 1 task failed:
/home/medha/var-fslc-yocto/sources/meta-webkit/recipes-browser/wpewebkit/wpewebkit_2.32.1.bb:do_compile
Summary: There were 2 WARNING messages shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code

 

0 件の賞賛
返信
1 解決策
10,863件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Muthyam,

I hope you are doing well.

I couldn't see any error related to the compilation of source code from logs.

This issue may arise due to not having enough memory. 

Please make sure that you have installed all dependencies required for yocto dunfell.
Please refer to installing the required packages.

For fsl-image-qt5 image one can also look at qtwebkit-based browsers.
Please refer to section 4 - Accelerated browsers support in Adding packages to the Yocto build

Thanks & Regards,
Dhruvit Vasavada

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
10,905件の閲覧回数
Muthyam
Contributor I

I added the line in local.conf, the problem remains even after adding the line

0 件の賞賛
返信
10,937件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Muthyam,

I hope you are doing well.

Please make sure that you have correctly set up the yocto project and added meta-qt5(dunfell version) layer.

Please add the below lines in local.conf

IMAGE_INSTALL_append = " wpewebkit cog imx-gst1.0-plugin"                                                                     

SKIP_META_VIRT_SANITY_CHECK = 1
#add the above line if virtualization support is not required.

 

Please make sure that you have enough memory on the host PC.

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信
10,886件の閲覧回数
Muthyam
Contributor I

I included this

IMAGE_INSTALL_append = " wpewebkit cog imx-gst1.0-plugin"

line my local.conf file and rebuilt the image using bitbake fsl-image-qt5, but the same error reappears. And another thing that I forget to mention is that when I enter bitbake fsl-image-qt5, the system freezes and by the time the system returns to normal, an error occurs.

 
 
0 件の賞賛
返信
10,864件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Muthyam,

I hope you are doing well.

I couldn't see any error related to the compilation of source code from logs.

This issue may arise due to not having enough memory. 

Please make sure that you have installed all dependencies required for yocto dunfell.
Please refer to installing the required packages.

For fsl-image-qt5 image one can also look at qtwebkit-based browsers.
Please refer to section 4 - Accelerated browsers support in Adding packages to the Yocto build

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信
10,767件の閲覧回数
Muthyam
Contributor I

Issue cleared now, it occurred because of less memory only.

Thank You.

0 件の賞賛
返信
10,751件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Muthyam,

I hope you are doing well.

As this issue is resolved, can I mark this case as close?

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信
10,298件の閲覧回数
Muthyam
Contributor I
yes
0 件の賞賛
返信