[Yocto BSP 1.8] i.MX6DP Display issue on LVDS dual channel panel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Yocto BSP 1.8] i.MX6DP Display issue on LVDS dual channel panel

1,865 Views
charleshuang
Senior Contributor II

u-boot setting:

setenv mmcargs setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot} ${bootargs} video=mxcfb0:dev=ldb,if=RGB24 fbmem=24M

 

LVDS dual channel setting in dts file:

&ldb {

  status = "okay";

};

 

&mxcfb1 {

  status = "okay";

};

 

&mxcfb2 {

  disp_dev = "ldb";

  mode_str ="1280x1024M@60";

  status = "okay";

};

 

&mxcfb3 {

  disp_dev = "ldb";

  mode_str ="1280x1024M@60";

  status = "okay";

};

 

&ldb {

  ext_ref = "true";

  status = "okay";

  split-mode;

 

  lvds-channel@0 {

  fsl,data-mapping = "spwg";

  fsl,data-width = <24>;

  crtc = "ipu2-di0";

  primary;

  status = "okay";

 

  display-timings {

                        native-mode = <&timing0>;

                        timing0: g190eg01v1 {

                                clock-frequency = <54000000>;

                                hactive = <640>;

                                vactive = <1024>;

                                hback-porch = <108>;

                                hfront-porch = <40>;

                                vback-porch = <3>;

                                vfront-porch = <29>;

                                hsync-len = <68>;

                                vsync-len = <7>;

                        };

                };

  };

 

  lvds-channel@1 {

                fsl,data-mapping = "spwg";

                fsl,data-width = <24>;

                crtc = "ipu1-di1";

                status = "okay";

 

  display-timings {

                        native-mode = <&timing1>;

                        timing1: g190eg01v1 {

                                clock-frequency = <54000000>;

                                hactive = <640>;

                                vactive = <1024>;

                                hback-porch = <108>;

                                hfront-porch = <40>;

                                vback-porch = <3>;

                                vfront-porch = <29>;

                                hsync-len = <68>;

                                vsync-len = <7>;

                        };

                };

  };

};

 

When the device display QT window on LVDS dual channel panel (1280*1024 resolution), the quality of the image is very poor.

Please see attached file.

Can you tell me how to modify dts file?

 

Thank you.

Original Attachment has been moved to: lvds_pictures.zip

0 Kudos
Reply
4 Replies

1,049 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Which BSP version are you using?

Are you trying to get an extended desktop or just clone the desktop?

Best Regards,

Alejandro

0 Kudos
Reply

1,049 Views
charleshuang
Senior Contributor II

Hi alejandrolozano,

I use BSP version is 3.14.52.

No. I just want to display QT desktop on a dual channel of lvds panel.

Thanks.

Best Regards,

Alex

0 Kudos
Reply

1,049 Views
强王
Contributor IV
this is my dts config:
  lvds_display: fb@0 {

        compatible = "fsl,mxc_sdc_fb";

        disp_dev = "ldb";

        interface_pix_fmt = "RGB24";

        mode_str ="LDB-XGA";

        default_bpp = <32>;

        int_clk = <0>;

        late_init = <0>;

        status = "okay";

    };

&ldb {

    status = "okay";

    split-mode;

    lvds-channel@0 {

        reg = <0>;

        crtc = "ipu2-di0";

        fsl,data-mapping = "spwg";

        fsl,data-width = <24>;

        status = "okay";

        display-timings {

            native-mode = <&timing0>;

            timing0: g104xvn01 {

                clock-frequency = <130000000>;

                hactive = <1920>;

                vactive = <720>;

                hback-porch = <40>;

                hfront-porch = <40>;

                vback-porch = <15>;

                vfront-porch = <15>;

                hsync-len = <80>;

                vsync-len = <10>;

            };

        };

    };

    lvds-channel@1 {

        reg = <1>;

        crtc = "ipu2-di1";

        fsl,data-mapping = "spwg";

        fsl,data-width = <24>;

        status = "okay";

        primary;

        display-timings {

            native-mode = <&timing1>;

            timing1: g104xvn01 {

                clock-frequency = <130000000>;

                hactive = <1920>;

                vactive = <720>;

                hback-porch = <40>;

                hfront-porch = <40>;

                vback-porch = <15>;

                vfront-porch = <15>;

                hsync-len = <80>;

                vsync-len = <10>;                                                                                                                            

            };

        };

    };

};

0 Kudos
Reply

1,049 Views
charleshuang
Senior Contributor II

I try your method, it also cannot work. It works fine on i.MX6. But this issue is occurred  on i.MX6DP.

Can you tell me how to solve this issue on i.MX6DP?

Thanks.

0 Kudos
Reply