[Yocto BSP 1.8_ga] i.MX6DP The USB/USB OTG port cannot automatic mount the directory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Yocto BSP 1.8_ga] i.MX6DP The USB/USB OTG port cannot automatic mount the directory

1,819 Views
charleshuang
Senior Contributor II

When the USB disk is inserted USB/USB OTG port, it cannot automatic mount the directory.

But the device can detect this device (/dev/sda).

Console log:

     1) log of the USB disk is inserted USB port:

usb 1-1.4: new high-speed USB device number 3 using ci_hdrc

usb-storage 1-1.4:1.0: USB Mass Storage device detected

scsi1 : usb-storage 1-1.4:1.0

scsi 1:0:0:0: Direct-Access     JetFlash Transcend 16GB   8.07 PQ: 0 ANSI: 4

sd 1:0:0:0: [sda] 30530688 512-byte logical blocks: (15.6 GB/14.5 GiB)

sd 1:0:0:0: [sda] Write Protect is off

sd 1:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA

usb 1-1.4: reset high-speed USB device number 3 using ci_hdrc

usb 1-1.4: reset high-speed USB device number 3 using ci_hdrc

usb 1-1.4: reset high-speed USB device number 3 using ci_hdrc

usb 1-1.4: reset high-speed USB device number 3 using ci_hdrc

usb 1-1.4: reset high-speed USB device number 3 using ci_hdrc

usb 1-1.4: reset high-speed USB device number 3 using ci_hdrc

usb 1-1.4: reset high-speed USB device number 3 using ci_hdrc

sd 1:0:0:0: [sda] Media Changed

sd 1:0:0:0: [sda] 

Result: hostbyte=DID_OK driverbyte=DRIVER_SENSE

sd 1:0:0:0: [sda] 

Sense Key : Unit Attention [current]

Info fld=0x0

sd 1:0:0:0: [sda] 

Add. Sense: Not ready to ready change, medium may have changed

sd 1:0:0:0: [sda] CDB:

Read(10): 28 00 00 00 00 00 00 00 08 00

end_request: I/O error, dev sda, sector 0

Buffer I/O error on device sda, logical block 0

sda: unable to read partition table

hub 1-1:1.0: cannot reset port 4 (err = -71)

usb 1-1.4: USB disconnect, device number 3

sd 1:0:0:0: [sda] READ CAPACITY failed

sd 1:0:0:0: [sda] 

Result: hostbyte=DID_NO_CONNECT driverbyte=DRIVER_OK

sd 1:0:0:0: [sda] Sense not available.

sd 1:0:0:0: [sda] Write Protect is on

sd 1:0:0:0: [sda] No Caching mode page found

sd 1:0:0:0: [sda] Assuming drive cache: write through

sd 1:0:0:0: [sda] Attached SCSI removable disk

sd 1:0:0:0: [sda] Asking for cache data failed

scsi 1:0:0:0: [sda] Assuming drive cache: write through

usb 1-1.4: new high-speed USB device number 4 using ci_hdrc

usb-storage 1-1.4:1.0: USB Mass Storage device detected

scsi2 : usb-storage 1-1.4:1.0

scsi 2:0:0:0: Direct-Access     JetFlash Transcend 16GB   8.07 PQ: 0 ANSI: 4

sd 2:0:0:0: [sda] 30530688 512-byte logical blocks: (15.6 GB/14.5 GiB)

sd 2:0:0:0: [sda] Write Protect is off

sd 2:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA

sda: sda1

sd 2:0:0:0: [sda] Attached SCSI removable disk

usb 1-1.4: reset high-speed USB device number 4 using ci_hdrc

sd 2:0:0:0: [sda] Media Changed

sd 2:0:0:0: [sda] 

Result: hostbyte=DID_OK driverbyte=DRIVER_SENSE

sd 2:0:0:0: [sda] 

Sense Key : Unit Attention [current]

Info fld=0x0

sd 2:0:0:0: [sda] 

Add. Sense: Not ready to ready change, medium may have changed

sd 2:0:0:0: [sda] CDB:

Read(10): 28 00 00 00 00 20 00 00 18 00

end_request: I/O error, dev sda, sector 32

Buffer I/O error on device sda, logical block 4

Buffer I/O error on device sda, logical block 5

Buffer I/O error on device sda, logical block 6

sda: sda1

root@:~#

root@:~# df -h

Filesystem      Size  Used Avail Use% Mounted on

/dev/root       3.4G  3.3G     0 100% /

devtmpfs        503M   76K  503M   1% /dev

tmpfs            40K     0   40K   0% /mnt/.psplash

tmpfs           503M  256K  503M   1% /run

tmpfs           503M   96K  503M   1% /var/volatile

/dev/mmcblk0p1  8.0M  5.4M  2.7M  67% /run/media/mmcblk0p1

/dev/mmcblk2p1  8.0M  5.4M  2.7M  67% /run/media/mmcblk2p1

/dev/mmcblk0p2  3.4G  1.5G  1.7G  47% /run/media/mmcblk0p2

root@:~# ls /dev/sda

sda   sda1 

     2) log of the USB disk is inserted USB OTG port:

ci_hdrc ci_hdrc.0: EHCI Host Controller

ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 2

ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

usb 2-1: new high-speed USB device number 2 using ci_hdrc

usb-storage 2-1:1.0: USB Mass Storage device detected

scsi1 : usb-storage 2-1:1.0

scsi 1:0:0:0: Direct-Access     JetFlash Transcend 16GB   8.07 PQ: 0 ANSI: 4

sd 1:0:0:0: [sda] 30530688 512-byte logical blocks: (15.6 GB/14.5 GiB)

sd 1:0:0:0: [sda] Write Protect is off

sd 1:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA

sda: sda1

sd 1:0:0:0: [sda] Attached SCSI removable disk

usb 2-1: reset high-speed USB device number 2 using ci_hdrc

sd 1:0:0:0: [sda] Media Changed

sd 1:0:0:0: [sda] 

Result: hostbyte=DID_OK driverbyte=DRIVER_SENSE

sd 1:0:0:0: [sda] 

Sense Key : Unit Attention [current]

Info fld=0x0

sd 1:0:0:0: [sda] 

Add. Sense: Not ready to ready change, medium may have changed

sd 1:0:0:0: [sda] CDB:

Read(10): 28 00 01 d1 dc 7d 00 00 01 00

end_request: I/O error, dev sda, sector 30530685

Buffer I/O error on device sda, logical block 3816335

sda: sda1

FAT-fs (sda1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.

root@:~#

root@:~# df -h

Filesystem      Size  Used Avail Use% Mounted on

/dev/root       3.4G  3.3G     0 100% /

devtmpfs        503M   76K  503M   1% /dev

tmpfs            40K     0   40K   0% /mnt/.psplash

tmpfs           503M  256K  503M   1% /run

tmpfs           503M   96K  503M   1% /var/volatile

/dev/mmcblk0p1  8.0M  5.4M  2.7M  67% /run/media/mmcblk0p1

/dev/mmcblk2p1  8.0M  5.4M  2.7M  67% /run/media/mmcblk2p1

/dev/mmcblk0p2  3.4G  1.5G  1.7G  47% /run/media/mmcblk0p2

root@:~# ls /dev/sda

sda   sda1

Can you help me to solve this issue?

Thank you.

Best Regards,

Alex

Labels (3)
0 Kudos
Reply
2 Replies

988 Views
art
NXP Employee
NXP Employee

This is just a regular behaviour, not specific to any NXP product. Just google for "auto mounting removable device in Linux". The example answers are as follows:

https://help.ubuntu.com/community/Mount/USB

http://superuser.com/questions/455597/how-to-mount-removable-media-in-media-label-automatically-when...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

988 Views
charleshuang
Senior Contributor II

I think you misunderstood what I meant.

The i.MX6 product doesn't happen this issue on Yocto BSP 1.8_ga.

But the i.MX6DP product will happen this issue.

I try to manual mount USB disk, it still cannot mount the directory.

Do you have other suggestion?

Thanks.

0 Kudos
Reply