Yocto Adb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto Adb

4,580 Views
li_hong
Contributor III

Hi, Team:

   As you know, Adb is a convenient tool chain in Android system.

   How to porting Adb module to Yocto.

Board:imx6ull   

Kernel:4.14.78

Thank you in advance.

Labels (2)
3 Replies

4,266 Views
zhufeng1006
Contributor I

Hi,have you finished adb porting? Is there any document or advise?

BR,

Dustin

0 Kudos
Reply

4,266 Views
karangajjar
Senior Contributor II

Hi hong li,

Please follow Android user guide of the particular android version you are using. You can build the images for three modes: eng, user, userdebug. These modes will have adb enable/disable by default.

https://www.nxp.com/docs/en/supporting-information/android_p9.0.0_2.0.0-ga_docs.zip 

Regards,

Karan Gajjar

4,266 Views
igorpadykov
NXP Employee
NXP Employee

Hi hong

one can try to follow sect.7.2.1 Using ADB Android User's Guide

included in Android P9.0.0_2.2.0 Documentation

general Android tutorials

Android Debug Bridge (adb)  |  Android Developers 

Running and Debugging Your Android Application On a Remote Android Device - RAD Studio 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------