Xip Bee Bootloader Bug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Xip Bee Bootloader Bug

1,103 Views
leoqian
Contributor I

Hello, I recently discovered an issue with BEE XIP encryption while debugging the RT1021 chip. My program structure is to write a bootloader myself (address: 0x6000000-0x60040000), and then load the APP to start (address: 0x60040000 0x6040000). The bootloader itself uses XIP BEE encryption to start, and then loads the APP and configures BEE to the APP startup area, achieving encrypted operation of both the bootloader and the App. The problem now is that even if the bootloader itself is not suitable for bee encryption, it runs normally. Once the bootloader uses bee encryption, the program will encounter inexplicable problems. Sometimes it can run normally, and sometimes modifying one or two lines of code can cause it to run away. I hope the engineers from the original factory can help analyze where the problem may be.

0 Kudos
Reply
1 Reply

1,072 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

 

Thank you in advance for contacting NXP support.

We have the following document that will help you out with the BEE XIP configuration this is based for RT10xx products please let me know if this guide was useful.

0 Kudos
Reply