Xfbdev

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,301件の閲覧回数
alexandrglukhov
Contributor III

Hello, I have i.MX28 and I'm using Buildroot. Everything was ok, until I decide to clean file system with

make clean

and then make it again with

make.

Now, when I write:

Xfbdev -mouse tslib,2,device=/dev/input/event0 &

I get

Xfbdev: command not found

I think, I set the same configurations, but it seems, it different. Can you help me with it? Which package, library or element needs for Xfbdev working? Maybe need special version of gcc or other?

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
3,776件の閲覧回数
alexandrglukhov
Contributor III

There are two X.Org servers in buildroot: Modular and Tiny/Kdrive. If I first choose modular and then do make, I have no Xfbdev. And if then I change to another server, I still have no Xfbdev. But if I do make clean and choose Tiny/Kdrive - then I get my Xfbdev. So, it's ok now, thank you.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,776件の閲覧回数
b36401
NXP Employee
NXP Employee

I have no idea what went wrong.
Please try to put attached file into /usr/bin/ directory of root filesystem.

3,776件の閲覧回数
alexandrglukhov
Contributor III

There are two X.Org servers in buildroot: Modular and Tiny/Kdrive. If I first choose modular and then do make, I have no Xfbdev. And if then I change to another server, I still have no Xfbdev. But if I do make clean and choose Tiny/Kdrive - then I get my Xfbdev. So, it's ok now, thank you.

0 件の賞賛
返信