Xfbdev with mouse and tslib is not working simultaneously

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Xfbdev with mouse and tslib is not working simultaneously

3,055件の閲覧回数
nagesha71
Contributor I

Hi,

I am working on the board i.mx53 SMD tablet, booted with 11.05 build
images.

Touch pad with Xfbdev is working fine with the below Xfbdev command.

Xfbdev -screen 1024x768 -mouse tslib,,device=/dev/input/ts0  &

When I use with -mouse option (as given below) to work mouse simultaneously with the touch screen,
touch screen is not working properly. Means,
for the contact on touchpad - the cursor points to wrong coordinates.
and for the release of contact - the cursor came to right coordinate (where the contact happened).

Xfbdev -mouse tslib,,device=/dev/input/ts0 -mouse mouse,2,device=/dev/input/mice&

When I use the mouse, its changing to mouse protocol, as shown in below message.

Switching to mouse protocol "imps/2"
Switching to mouse protocol "exps/2"
Switching to mouse protocol "bus"
Switching to mouse protocol "ps/2"


After this, once I do ts_calibrate again, the touch is working fine.

Is it possible to use touch and mouse simultaneously with Xfbdev server ?

Please suggest me in a way forward.

 

-Nagesh A

タグ(1)
0 件の賞賛
返信
1 返信

1,624件の閲覧回数
MaciejSuminski
Contributor I

Maybe it is a bit outdated, but still there's the answer:

Xfbdev :0 -screen 480x800 -mouse tslib,1,device=/dev/input/ts0 -mouse mouse,2,device=/dev/input/mice &

It is working imx.51 with USB mouse and touchscreen

0 件の賞賛
返信