Xen support on Imx 8mplus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Xen support on Imx 8mplus

2,229 Views
MEGHANAB
Contributor I

Is it possible to port xen on to imx8mp 8mplus board but the board doesn’t have IOMMU.What are the hypervisors that can be ported to imx 8mplus board please explain the workflow properly 

0 Kudos
Reply
3 Replies

2,201 Views
MEGHANAB
Contributor I
Hello, I'm porting jailhouse hypervisor onto i.MX 8M PLus board.So may i know the correct procedure to do so and do we have any prebuilt yocto wic images for i.MX 8M PLus,prebuilt linux kernel if yes please provide the source links.
Regards
MEGHANAB
Tags (1)
0 Kudos
Reply

2,193 Views
jamesbone
NXP TechSupport
NXP TechSupport

For building the Xen and Jailhouse, please refer to Chapter 5.6.11 and 5.6.12 in Yocto User's Guide.

https://www.nxp.com.cn/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf

0 Kudos
Reply

2,214 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @MEGHANAB 

I hope you are doing very well.

 

Xen is only supported by i.MX95 as you can see on i.MX Linux User's Guide, chapter 17.2 Xen hypervisor.

But you can use Jailhouse hypervisor, more details on the same guide on chapter 17.1 Jailhouse hypervisor.

 

Best regards,

Salas.

0 Kudos
Reply