Xen 6.6 compatibility with Linux kernel 6.6 on i.MX8QXP platform

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Xen 6.6 compatibility with Linux kernel 6.6 on i.MX8QXP platform

562 次查看
subash_p
Contributor III

I'm trying to build the Linux kernel version 6.6 and the Xen hypervisor version 6.6 from NXP's source. Is it possible to run Xen 6.6 on the Linux kernel 6.6 for the i.MX8QXP platform? Are there any known issues or patches required for compatibility?

0 项奖励
回复
3 回复数

540 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

 

 

 Is it possible to run Xen 6.6 on the Linux kernel 6.6 for the i.MX8QXP platform?

A:Yes,  but for the Linux kernel 6.6 we released do not support the Xen hypervisor, you can refer to the old version BSP and porting it.

Sorry we do not have this document for you, 

Rita_Wang_0-1747279110722.png

 

Embedded Linux for i.MX Applications Processors | NXP Semiconductors

Hope this can do help for you

Wish you have a nice day

Best Regards

Rita

0 项奖励
回复

521 次查看
subash_p
Contributor III

Hi @Rita_Wang 

Thank you for your quick response. When I tried to flash the Linux version 6.6 with Xen 6.6, I faced some errors in the kernel console, and it's not booting up. I will attach the log where I faced an error below

0 项奖励
回复

464 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi @subash_p ,

For the Linux version 6.6 in default do not support the XEN, as I tell you that only the old version BSP support it, for the Linux version 6.6  you need to porting the XEN to it.

Wish you have a nice day

Best Regards

Rita

0 项奖励
回复