X11 Forwarding not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

X11 Forwarding not working

2,138 次查看
guna007
Contributor III

I recently upgraded from jethro branch to morty branch. After that, X11 forwarding is not working?

Notes:

Kernel: 4.1.x

Image: core-image-multimedia-full

Configuration: X11Forwarding is enabled in /etc/ssh/sshd_config file in the board.

标记 (3)
3 回复数

1,864 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello OtavioSalvador ‌, would you know if there is a known issue regarding this on the Morty branch?

Regards,

0 项奖励
回复

1,864 次查看
OtavioSalvador
Senior Contributor II

Hello gusarambula‌, I did fix this in past for a customer. If I recall correctly, the cause of the change was a more strict default setting from OpenSSH and I ended adjusting it for the customer's needs.

1,864 次查看
guna007
Contributor III

I found xauth is missing in the image . When I added that to image, it's working now!