Wrong imx6 fstab.freescale patch for SD card usage in Android jb43

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wrong imx6 fstab.freescale patch for SD card usage in Android jb43

3,065 次查看
mabel
Contributor I

Hello all,

i found a little typo in the user guide docs how to build android jb4.3 for SD card usage. The fstab.freescale patch is not correct, there some missing "-". Here is the right fstab.freescale to build android which can be booted from SD card. I've copied this from the jb43 demo image.

best regards,

Martin

# Android fstab file.

#<src>                                                  <mnt_point>         <type>    <mnt_flags and options>                       <fs_mgr_flags>

# The filesystem that contains the filesystem checker binary (typically /system) cannot

# specify MF_CHECK, and must come before any filesystems that do specify MF_CHECK

#/devices/platform/sdhci-esdhc-imx.2/mmc_host/mmc1 /mnt/extsd vfat defaults voldmanaged=sdcard:auto

/devices/platform/sdhci-esdhc-imx.1/mmc_host/mmc2 /mnt/extsd vfat defaults voldmanaged=sdcard:auto

/devices/platform/fsl-ehci /mnt/udisk vfat defaults voldmanaged=sdcard:auto

#/dev/block/mmcblk0p5    /system      ext4    ro                                                                               wait

#/dev/block/mmcblk0p4    /data        ext4    nosuid,nodev,nodiratime,noatime,nomblk_io_submit,noauto_da_alloc,errors=panic    wait,encryptable=footer

#/dev/block/mmcblk0p6    /cache       ext4    nosuid,nodev,nomblk_io_submit                                                    wait

#/dev/block/mmcblk0p7    /device      ext4    ro,nosuid,nodev                                                                  wait

#/dev/block/mmcblk0p1    /boot        emmc    defaults                                                                         defaults

#/dev/block/mmcblk0p2    /recovery    emmc    defaults                                                                         defaults

#/dev/block/mmcblk0p8    /misc        emmc    defaults                                                                         defaults

/dev/block/mmcblk1p5    /system      ext4    ro                                                                               wait

/dev/block/mmcblk1p4    /data        ext4    nosuid,nodev,nodiratime,noatime,nomblk_io_submit,noauto_da_alloc,errors=panic    wait,encryptable=footer

/dev/block/mmcblk1p6    /cache       ext4    nosuid,nodev,nomblk_io_submit                                                    wait

/dev/block/mmcblk1p7    /device      ext4    ro,nosuid,nodev                                                                  wait

/dev/block/mmcblk1p1    /boot        emmc    defaults                                                                         defaults

/dev/block/mmcblk1p2    /recovery    emmc    defaults                                                                         defaults

/dev/block/mmcblk1p8    /misc        emmc    defaults                                                                         defaults

标签 (2)
标记 (3)
0 项奖励
回复
0 回复数