Wrong confidence score Yolov8 on NPU i.MX 8M Plus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wrong confidence score Yolov8 on NPU i.MX 8M Plus

2,674 次查看
simoberny
Contributor III

Hi,

I've been successfully using yolov5 on NPU for a while now.
I tried to switch to Yolov8, but for now with partial success.

OS: Yocto Kirkstone, Kernel 5.15.71

Hardware: i.MX 8M Plus

With both networks my procedure is as follows:

  • Training with the Yolo tool on dataset created with Roboflow
  • Exporting the .pt (Pytorch) to .pb (TF GraphDef) using the export tool integrated in the two versions of Yolo
  • Convert .pb to .tflite using NXP eIQ Portal tool using quantization on input.

In the case of Yolov5 the inference works perfectly and I can get 18+ FPS using an input of 320x320.

In the case of Yolov8 instead (with the necessary adjustments for inference, row/col inversion etc...), I obtain the bounding boxes correctly, but with a confidence score always equal and greater than 1.

Is there anyone who has already seen this problem or anyone who has already worked successfully with this type of network?

 

Thanks in advance,

Best regards

0 项奖励
回复
2 回复数

2,438 次查看
HME15769
Contributor II

@simoberny 
Belatedly, I tried the export feature of the ultralytics package and obtained successful results.
However, the inference speed was still slow, even on the NPU.
https://docs.ultralytics.com/modes/export/

@JosephAtNXP 
Don't bother answering if you don't understand.

0 项奖励
回复

2,646 次查看
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

There are improves in different model executions when updating BSP, this would worth a try;

Also, the two models probably work with different pytorch versions and they're updated in some releases.

Could you try with latest BSP available?

Regards

0 项奖励
回复