Writing image to SCM-QWKS-REV2 using MFG tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Writing image to SCM-QWKS-REV2 using MFG tool

1,232 Views
aliismail
Contributor IV

I have been trying to use the MFG tool to write the stock image to the the eMMC on the SCM-QWKS board. I keep getting the following error:

UTP: sending Non-success to kernel for command $ echo 0 > /sys/block/mmcblk0boot0/force_ro.

I imagine my issue might simply be how the dip switches are oriented or if an SD card must be available for the tool to download the image. I have been able to load the linux image onto an SD card, however, I cannot on the eMMC. Is there any document specific to the SCM board? There are scripts available, but non write to the eMMC.

Labels (5)
0 Kudos
Reply
1 Reply

1,033 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ali

for eMMC one can look at i.MX6 SabreSD MfgTools script mfgtool2-yocto-mx-sabresd-emmc.vbs

i.MX 6 Series Software and Development Tool|NXP

there are some eMMC protection features described in

linux/Documentation/mmc/mmc-dev-parts.txt

one can try solutions on

i.MX6 and boot from eMMC - not working with MMC/eMMC config

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------