Write ubi android image from u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Write ubi android image from u-boot

2,495件の閲覧回数
mirkoardinghi1
Contributor IV


Hi

I made a android build with the official freescale bsp.

The images for the sd card works fine but i have some problems with the nand versions

How can I write the  android_root.img image?

I write as a raw image but when I boot the kernel doesn't find the /dev/ubi0_x partitions.

ラベル(4)
0 件の賞賛
返信
1 返信

2,365件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mirko

please look at sect.5.2 System on NAND for the SABRE-AI board attached Android User Guide

and mfg tools script mfgtool2-android-mx6dl-sabreauto-nand.vbs

Programmers (Flash, etc.) (12)

IMX6_M6.0.1_1.0.0_MFG_TOOL (REV M6.0.1_1.0.0)

i.MX 6 Family Manufacturing Toolkit for M6.0.1_1.0.0 (3.14 kernel)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信