Write kernel to nand via imx-usb-loader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Write kernel to nand via imx-usb-loader

2,108 Views
adi1525
Contributor III

Hello

I use Yocto and I writed u-boot to I.mx6ul witch use imx_usb_loader by USB debug mode, but I can't find information how write kernel and rootfs, is it posible ? or if I can write it with mfgtools ??

I don't have access to ethernet and USB/SD CARD.

By the way, is there option in uboot to program kernel or rootfs via WIFI ?

Regards,

Adrian

Labels (1)
0 Kudos
Reply
2 Replies

1,668 Views
adi1525
Contributor III

Hi Igor and thanks for reply. And what with boot with wifi ? because I have single module without ethernet and USB interface on board.

Regards

Adrian

0 Kudos
Reply

1,668 Views
igorpadykov
NXP Employee
NXP Employee

Hi Adrian

nxp does not support usb-loader, it was developed by third party, one can check

i.MX USB Loader 

Guide to flash iMX6 from Linux 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply