Windows embedded compact 2013 GPU source code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Windows embedded compact 2013 GPU source code

1,943件の閲覧回数
Jeslin
Contributor I

I am facing issue with IMX6 solo with 512 MB RAM, when I run GPU sample application with 512 MB ram it crashes after ~5-10secs. But the same crash doesn't  happen for 1GB RAM. I suspect the memory range used for GPU is hard coded in the driver may cause the crash issue. To debug this i need source code for GPU driver(IMX6) Windows Embedded Compact 2013.

Can I get the source code for GPU driver (IMX6) Windows Embedded compact 2013?

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,767件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

AdeneoEmbedded , do you have information or can you help with this question?

0 件の賞賛
返信

1,767件の閲覧回数
Jeslin
Contributor I

Hi Adeneo Embedded

Can you help me on this issue?

0 件の賞賛
返信