Windows embedded compact 2013 GPU source code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Windows embedded compact 2013 GPU source code

1,884 次查看
Jeslin
Contributor I

I am facing issue with IMX6 solo with 512 MB RAM, when I run GPU sample application with 512 MB ram it crashes after ~5-10secs. But the same crash doesn't  happen for 1GB RAM. I suspect the memory range used for GPU is hard coded in the driver may cause the crash issue. To debug this i need source code for GPU driver(IMX6) Windows Embedded Compact 2013.

Can I get the source code for GPU driver (IMX6) Windows Embedded compact 2013?

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,708 次查看
SergioSolis
NXP Employee
NXP Employee

AdeneoEmbedded , do you have information or can you help with this question?

0 项奖励
回复

1,708 次查看
Jeslin
Contributor I

Hi Adeneo Embedded

Can you help me on this issue?

0 项奖励
回复