Windows CE 6.0 on i.Mx6?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Windows CE 6.0 on i.Mx6?

跳至解决方案
6,808 次查看
filippob
Contributor I

Hi all,

does anyone foresee (or know that exists) a Windows Embedded CE 6.0 BSP for any of the i.Mx6 boards?

Thanks

Filippo

标签 (2)
1 解答
3,439 次查看
jimmychan
NXP TechSupport
NXP TechSupport

For i.MX6 WinCE BSP, you may need to contact other companies. e.g. iWave Systems.

https://community.freescale.com/thread/295802

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,092 次查看
coffani_luigi
Contributor I

thanks for the replies

0 项奖励
回复
3,439 次查看
dantx
Contributor I

Toradex also provides a WinCE / Windows Embedded Compact 7 and 2013 for the I.MX6 modules:

https://www.toradex.com/operating-systems/windows-ce

https://www.toradex.com/computer-on-modules

http://developer.toradex.com/frequent-downloads#Colibri_IMX6_and_Apalis_IMX6

For the I.MX6 it is only WEC7 or WEC2013. One of the reason is that WinCE6 only supports single core, so the use on the dual and quad I.MX6 is limited. WinCE 6.0 is supported on other Freescale SoCs like the Vybrid VF50 and VF61.

In general the update form WinCE6 to WEC7 is easy. If you run binaries build for WinCE6.0, WEC7 will lock them to the first core so you will not have issues in case your program did not consider multicore use cases.

0 项奖励
回复
3,440 次查看
jimmychan
NXP TechSupport
NXP TechSupport

For i.MX6 WinCE BSP, you may need to contact other companies. e.g. iWave Systems.

https://community.freescale.com/thread/295802

0 项奖励
回复
3,439 次查看
filippob
Contributor I

thanks for the prompt replies,

I can see plenty of interesting WEC 7 board support packages, but what about WinCE 6.0?

0 项奖励
回复