Windows CE 6.0 on i.Mx6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows CE 6.0 on i.Mx6?

Jump to solution
6,016 Views
filippob
Contributor I

Hi all,

does anyone foresee (or know that exists) a Windows Embedded CE 6.0 BSP for any of the i.Mx6 boards?

Thanks

Filippo

Labels (2)
1 Solution
2,647 Views
jimmychan
NXP TechSupport
NXP TechSupport

For i.MX6 WinCE BSP, you may need to contact other companies. e.g. iWave Systems.

https://community.freescale.com/thread/295802

View solution in original post

0 Kudos
5 Replies
1,300 Views
coffani_luigi
Contributor I

thanks for the replies

0 Kudos
2,647 Views
dantx
Contributor I

Toradex also provides a WinCE / Windows Embedded Compact 7 and 2013 for the I.MX6 modules:

https://www.toradex.com/operating-systems/windows-ce

https://www.toradex.com/computer-on-modules

http://developer.toradex.com/frequent-downloads#Colibri_IMX6_and_Apalis_IMX6

For the I.MX6 it is only WEC7 or WEC2013. One of the reason is that WinCE6 only supports single core, so the use on the dual and quad I.MX6 is limited. WinCE 6.0 is supported on other Freescale SoCs like the Vybrid VF50 and VF61.

In general the update form WinCE6 to WEC7 is easy. If you run binaries build for WinCE6.0, WEC7 will lock them to the first core so you will not have issues in case your program did not consider multicore use cases.

0 Kudos
2,648 Views
jimmychan
NXP TechSupport
NXP TechSupport

For i.MX6 WinCE BSP, you may need to contact other companies. e.g. iWave Systems.

https://community.freescale.com/thread/295802

0 Kudos
2,647 Views
filippob
Contributor I

thanks for the prompt replies,

I can see plenty of interesting WEC 7 board support packages, but what about WinCE 6.0?

0 Kudos