Windows 10 IoT LVDS Resolution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows 10 IoT LVDS Resolution

Jump to solution
1,521 Views
hankwang
Contributor V

Hi , I have an Innolux g101ice-I01 panel with 1280x800 resolution. I tried to modify edid parameters in the galcore.inf. The screen will turn black when the system enters Windows. 

Does modifying the resolution only need to be modified in galcore.inf? Or are there other places that need to be modified? Please help to check the edid file for 1280x800.

Please refer to the attachment for the edid parameter.

Note: The original galcore.inf resolution can normal display (1280x720). But the bottom of screen has overlay screen.

Here is innolux_g101ice_l01_timing. I set pixel clock to 71.1Mhz.

static const struct display_timing innolux_g101ice_l01_timing = {
	.pixelclock = { 60400000, 71100000, 74700000 },
	.hactive = { 1280, 1280, 1280 },
	.hfront_porch = { 41, 80, 100 },
	.hback_porch = { 40, 79, 99 },
	.hsync_len = { 1, 1, 1 },
	.vactive = { 800, 800, 800 },
	.vfront_porch = { 5, 11, 14 },
	.vback_porch = { 4, 11, 14 },
	.vsync_len = { 1, 1, 1 },
	.flags = DISPLAY_FLAGS_DE_HIGH,
};

Thanks.

0 Kudos
Reply
1 Solution
1,471 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @hankwang,

I hope you are doing well
 
The information related to the same for the HDMI/ LVDS/ MIPI-DSI display is mentioned in detail in Chapter 3 Display/GPU driver of the document i.MX Windows 10 IoT User’s Guide
 
Thanks & Regards,
Dhruvit Vasavada

View solution in original post

0 Kudos
Reply
2 Replies
1,472 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @hankwang,

I hope you are doing well
 
The information related to the same for the HDMI/ LVDS/ MIPI-DSI display is mentioned in detail in Chapter 3 Display/GPU driver of the document i.MX Windows 10 IoT User’s Guide
 
Thanks & Regards,
Dhruvit Vasavada
0 Kudos
Reply
1,430 Views
hankwang
Contributor V

Thank you for the information. This problem can be fixed.

0 Kudos
Reply