Windows 10 IoT Enterprise source cannot be downloaded.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows 10 IoT Enterprise source cannot be downloaded.

2,284 Views
okuda
Contributor III

I can't automatically jump to the following URL and download it.

https://cache.nxp.com/secured/bsps/W21H2-1-4-1-imx-windows-bsp.zip?__gda__=1690942842_fdb8ccb8642159...

Attached is a screenshot of when the error occurs.
(Although it is displayed in Japanese)

0 Kudos
Reply
4 Replies

2,220 Views
joanxie
NXP TechSupport
NXP TechSupport

I got reply from web team that the link is fixed

0 Kudos
Reply

2,227 Views
michal_hromadka
NXP Employee
NXP Employee

Hello @okuda,

The link to the BSP souce code should be working now.

Regards,

Michal 

0 Kudos
Reply

2,205 Views
okuda
Contributor III

Hello Michal  Joanxie

Thank you for your response.
I was able to download normally.

Regards,

Koji Okuda

0 Kudos
Reply

2,255 Views
joanxie
NXP TechSupport
NXP TechSupport

the web team will check this and I will update here

0 Kudos
Reply