Windows 10 IOT eMMC Flash Failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Windows 10 IOT eMMC Flash Failure

1,938件の閲覧回数
Zaid_Noordeen
Contributor II

Hi, We are working in Windows 10 IOT on iMX6DL. We needs to flash the eMMC to enable eMMC boot. We can see all the required partitions are getting created similar to SD in eMMC too. But, when we change the boot switch to eMMC boot, eMMC booting with older U-Boot which is not related to this Windows 10 IOT. On closer inspection, we find out that force_ro is not disabled resulting in BootLoader(firmware_fit.merged) is not getting flashed to eMMC. We used Linux MFG tool to flash that part alone to eMMC, then eMMC boots with Windows 10 IOT image. Our question is, why dism tool not able to write into that protected area which can be written using MFG tool? and is there a way to avoid using MFG tool to flash that protected boot partition? 

ラベル(3)
0 件の賞賛
返信
1 返信

1,881件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

currently nxp doesn't support Windwos IOT anymore, any further questions, pls contact Microsoft directly

0 件の賞賛
返信