Windows 10 IOT eMMC Flash Failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows 10 IOT eMMC Flash Failure

1,929 Views
Zaid_Noordeen
Contributor II

Hi, We are working in Windows 10 IOT on iMX6DL. We needs to flash the eMMC to enable eMMC boot. We can see all the required partitions are getting created similar to SD in eMMC too. But, when we change the boot switch to eMMC boot, eMMC booting with older U-Boot which is not related to this Windows 10 IOT. On closer inspection, we find out that force_ro is not disabled resulting in BootLoader(firmware_fit.merged) is not getting flashed to eMMC. We used Linux MFG tool to flash that part alone to eMMC, then eMMC boots with Windows 10 IOT image. Our question is, why dism tool not able to write into that protected area which can be written using MFG tool? and is there a way to avoid using MFG tool to flash that protected boot partition? 

Labels (3)
0 Kudos
Reply
1 Reply

1,872 Views
joanxie
NXP TechSupport
NXP TechSupport

currently nxp doesn't support Windwos IOT anymore, any further questions, pls contact Microsoft directly

0 Kudos
Reply