WinCE 6.0 how do i change the default boot settings?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

WinCE 6.0 how do i change the default boot settings?

1,461 次查看
RobertA
Contributor I

Hello,

In WinCE 6.0 how do i change the default boot settings such as the following listed below?

DHCP: Disable

IP Address: 10.101.20.1

IP Mask: 255.255.0.0

Select Boot Device: NK from SD/MMC

KITL Enable Mode: Disable

标签 (2)
0 项奖励
回复
1 回复

1,136 次查看
Yuri
NXP Employee
NXP Employee

It is needed to change and rebuild Eboot. Eboot sources may be found in directory 

c:\WINCE600\PLATFORM\iMX51-EVK-PDK1_7\SRC\BOOTLOADER\

0 项奖励
回复