WinCE 6.0 how do i change the default boot settings?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WinCE 6.0 how do i change the default boot settings?

1,407 Views
RobertA
Contributor I

Hello,

In WinCE 6.0 how do i change the default boot settings such as the following listed below?

DHCP: Disable

IP Address: 10.101.20.1

IP Mask: 255.255.0.0

Select Boot Device: NK from SD/MMC

KITL Enable Mode: Disable

Labels (2)
0 Kudos
Reply
1 Reply

1,082 Views
Yuri
NXP Employee
NXP Employee

It is needed to change and rebuild Eboot. Eboot sources may be found in directory 

c:\WINCE600\PLATFORM\iMX51-EVK-PDK1_7\SRC\BOOTLOADER\

0 Kudos
Reply